IMU - Inertial Measurement UnitBSP > Thunderboard Sense BSP
Detailed Description
Inertial Measurement Unit driver.
| Data Structures | |
| struct | _IMU_SensorFusion | 
| Structure to store the sensor fusion data. | |
| Typedefs | |
| typedef struct _IMU_SensorFusion | IMU_SensorFusion | 
| Structure to store the sensor fusion data. | |
| Functions | |
| void | IMU_accelerationGet (int16_t avec[3]) | 
| Retrieves the processed acceleration data. | |
| void | IMU_clearDataReadyFlag (void) | 
| Clears the IMU data ready flag. In case of ver 0.3.0 and older of the PIC firmware the interrupt register also needs to be cleared. | |
| void | IMU_config (float sampleRate) | 
| Configures the IMU. | |
| void | IMU_dcmGetAngles (float dcm[3][3], float angle[3]) | 
| Calculates the Euler angles (roll, pitch, yaw) from the DCM matrix. | |
| void | IMU_dcmNormalize (float dcm[3][3]) | 
| Normalizes the DCM matrix. | |
| void | IMU_dcmReset (float dcm[3][3]) | 
| Sets the elements of the DCM matrixto the corresponding elements of the identity matrix. | |
| void | IMU_dcmResetZ (float dcm[3][3]) | 
| DCM reset, Z direction. | |
| void | IMU_dcmRotate (float dcm[3][3], float angle[3]) | 
| Rotates the DCM matrix by a given angle. | |
| uint32_t | IMU_deInit (void) | 
| De-initializes the IMU chip. | |
| void | IMU_fuseAccelerometerSetSampleRate ( IMU_SensorFusion *f, float rate) | 
| Sets the accelerometer sample rate in the IMU_SensorFusion structure. | |
| void | IMU_fuseAccelerometerUpdateFilter ( IMU_SensorFusion *f, float avec[3]) | 
| The current accelerometer data is added to the accumulator. | |
| void | IMU_fuseGyroCorrection ( IMU_SensorFusion *f, bool accValid, bool dirValid, float dirZ) | 
| Calculates the gyro correction vector. | |
| void | IMU_fuseGyroCorrectionClear ( IMU_SensorFusion *f) | 
| Clears the gyro correction vector. | |
| void | IMU_fuseGyroSetSampleRate ( IMU_SensorFusion *f, float rate) | 
| Sets the gyro sample rate and related values in the IMU_SensorFusion structure. | |
| void | IMU_fuseGyroUpdate ( IMU_SensorFusion *f, float gvec[3]) | 
| Updates the fusion calculation with a new gyro data. | |
| void | IMU_fuseNew ( IMU_SensorFusion *f) | 
| Initializes a new IMU_SensorFusion structure. | |
| void | IMU_fuseReset ( IMU_SensorFusion *f) | 
| Clears the values of the sensor fusion object. | |
| void | IMU_fuseUpdate ( IMU_SensorFusion *f) | 
| Updates the fusion calculation. | |
| void | IMU_getAccelerometerData (float avec[3]) | 
| Retrieves the raw acceleration data from the IMU. | |
| void | IMU_getGyroCorrectionAngles (float acorr[3]) | 
| Retrieves the processed gyroscope correction angles. | |
| void | IMU_getGyroData (float gvec[3]) | 
| Retrieves the raw gyroscope data from the IMU. | |
| uint8_t | IMU_getState (void) | 
| Returns IMU state. | |
| uint32_t | IMU_gyroCalibrate (void) | 
| Performs gyroscope calibration to cancel gyro bias. | |
| void | IMU_gyroGet (int16_t gvec[3]) | 
| Retrieves the processed gyroscope data. | |
| uint32_t | IMU_init (void) | 
| Initializes and calibrates the IMU. | |
| bool | IMU_isDataReady (void) | 
| Checks if there is new accel/gyro data available for read. | |
| bool | IMU_isDataReadyFlag (void) | 
| Checks if there is new accel/gyro data available for read. In case of ver 0.3.0 and older of the PIC firmware the state of the PIC_INT_WAKE needs to be read to determinte if the IMU interrupt is valid. | |
| void | IMU_matrixMultiply (float c[3][3], float a[3][3], float b[3][3]) | 
| Multiplies two 3x3 matrices. | |
| void | IMU_normalizeAngle (float *a) | 
| Normalizes the angle ( -PI < angle <= PI ) | |
| void | IMU_orientationGet (int16_t ovec[3]) | 
| Retrieves the processed orientation data. | |
| void | IMU_reset (void) | 
| Resets the fusion calculation. | |
| void | IMU_update (void) | 
| Gets a new set of data from the accel and gyro sensor and updates the fusion calculation. | |
| void | IMU_vectorAdd (float r[3], float a[3], float b[3]) | 
| Adds two vectors. | |
| void | IMU_vectorCrossProduct (float r[3], float a[3], float b[3]) | 
| Calculates the cross product of two vectors. | |
| float | IMU_vectorDotProduct (float a[3], float b[3]) | 
| Calculates the dot product of two vectors. | |
| void | IMU_vectorNormalizeAngle (float v[3]) | 
| Normalizes the angle of a vector. | |
| void | IMU_vectorScalarMultiplication (float r[3], float v[3], float scale) | 
| Multiplies a vector by a scalar. | |
| void | IMU_vectorScale (float v[3], float scale) | 
| Scales a vector by a factor. | |
| void | IMU_vectorSubtract (float r[3], float a[3], float b[3]) | 
| Subtracts vector b from vector a. | |
| void | IMU_vectorZero (float v[3]) | 
| Sets all elements of a vector to 0. | |
| Error Codes | |
| #define | IMU_OK 0 | 
| State Definitions | |
| #define | IMU_STATE_DISABLED 0x00 | 
| #define | IMU_STATE_READY 0x01 | 
| #define | IMU_STATE_INITIALIZING 0x02 | 
| #define | IMU_STATE_CALIBRATING 0x03 | 
Macro Definition Documentation
| #define IMU_OKÂ Â Â 0 | 
| #define IMU_STATE_CALIBRATINGÂ Â Â 0x03 | 
| #define IMU_STATE_DISABLEDÂ Â Â 0x00 | 
The IMU is disabled
        Definition at line
        
         56
        
        of file
        
         imu.h
        
        .
       
Referenced by IMU_deInit() , and IMU_init() .
| #define IMU_STATE_INITIALIZINGÂ Â Â 0x02 | 
The IMU is being initialized
        Definition at line
        
         58
        
        of file
        
         imu.h
        
        .
       
Referenced by IMU_config() , and IMU_init() .
| #define IMU_STATE_READYÂ Â Â 0x01 | 
The IMU is fully configured and ready to take measurements
        Definition at line
        
         57
        
        of file
        
         imu.h
        
        .
       
Referenced by IMU_config() , IMU_fuseUpdate() , IMU_getAccelerometerData() , IMU_getGyroData() , IMU_isDataReady() , and IMU_isDataReadyFlag() .
Function Documentation
| void IMU_accelerationGet | ( | int16_t | 
            avec[3]
            | ) | 
Retrieves the processed acceleration data.
- Parameters
- 
         [out] avecThree dimensonal acceleration vector 
- Returns
- None
        Definition at line
        
         231
        
        of file
        
         imu.c
        
        .
       
References _IMU_SensorFusion::aAccumulator , and _IMU_SensorFusion::aAccumulatorCount .
| void IMU_clearDataReadyFlag | ( | void | 
            | ) | 
Clears the IMU data ready flag. In case of ver 0.3.0 and older of the PIC firmware the interrupt register also needs to be cleared.
- Returns
- None
        Definition at line
        
         464
        
        of file
        
         imu.c
        
        .
       
References BOARD_imuClearIRQ() .
| void IMU_config | ( | float | 
            sampleRate
            | ) | 
Configures the IMU.
- Parameters
- 
         [in] sampleRateThe desired sample rate of the acceleration and gyro sensor 
- Returns
- None
IMU general use
        Definition at line
        
         165
        
        of file
        
         imu.c
        
        .
       
References BOARD_imuClearIRQ() , BOARD_imuEnableIRQ() , BOARD_imuSetIRQCallback() , ICM20648_ACCEL_BW_1210HZ , ICM20648_ACCEL_FULLSCALE_2G , ICM20648_accelBandwidthSet() , ICM20648_accelFullscaleSet() , ICM20648_accelSampleRateSet() , ICM20648_GYRO_BW_51HZ , ICM20648_GYRO_FULLSCALE_250DPS , ICM20648_gyroBandwidthSet() , ICM20648_gyroFullscaleSet() , ICM20648_gyroSampleRateSet() , ICM20648_interruptEnable() , ICM20648_interruptStatusRead() , ICM20648_lowPowerModeEnter() , ICM20648_sensorEnable() , IMU_fuseAccelerometerSetSampleRate() , IMU_fuseGyroSetSampleRate() , IMU_fuseReset() , IMU_STATE_INITIALIZING , IMU_STATE_READY , and UTIL_delay() .
Referenced by IMU_gyroCalibrate() .
| void IMU_dcmGetAngles | ( | float | 
            dcm[3][3],
            | 
| float | 
            angle[3]
            | ||
| ) | 
Calculates the Euler angles (roll, pitch, yaw) from the DCM matrix.
- Parameters
- 
         [in] dcmDCM matrix [out] angleAn array containing the Euler angles 
- Returns
- None
        Definition at line
        
         173
        
        of file
        
         imu_dcm.c
        
        .
       
Referenced by IMU_fuseGyroUpdate() .
| void IMU_dcmNormalize | ( | float | 
            dcm[3][3]
            | ) | 
Normalizes the DCM matrix.
- Parameters
- 
         dcmDCM matrix 
- Returns
- None
        Definition at line
        
         128
        
        of file
        
         imu_dcm.c
        
        .
       
References IMU_vectorAdd() , IMU_vectorCrossProduct() , IMU_vectorDotProduct() , and IMU_vectorScalarMultiplication() .
Referenced by IMU_fuseGyroUpdate() .
| void IMU_dcmReset | ( | float | 
            dcm[3][3]
            | ) | 
Sets the elements of the DCM matrixto the corresponding elements of the identity matrix.
Direction Cosine Matrix functions
- Parameters
- 
         dcmDCM matrix 
- Returns
- None
        Definition at line
        
         41
        
        of file
        
         imu_dcm.c
        
        .
       
Referenced by IMU_fuseReset() .
| void IMU_dcmResetZ | ( | float | 
            dcm[3][3]
            | ) | 
DCM reset, Z direction.
- Parameters
- 
         dcmDCM matrix 
- Returns
- None
        Definition at line
        
         64
        
        of file
        
         imu_dcm.c
        
        .
       
References IMU_vectorCrossProduct() , and IMU_vectorScale() .
| void IMU_dcmRotate | ( | float | 
            dcm[3][3],
            | 
| float | 
            angle[3]
            | ||
| ) | 
Rotates the DCM matrix by a given angle.
- Parameters
- 
         dcmDCM matrix angleRotation angle 
- Returns
- None
        Definition at line
        
         89
        
        of file
        
         imu_dcm.c
        
        .
       
References IMU_matrixMultiply() .
Referenced by IMU_fuseGyroUpdate() .
| uint32_t IMU_deInit | ( | void | 
            | ) | 
De-initializes the IMU chip.
- Returns
- Returns zero on OK, non-zero otherwise
        Definition at line
        
         133
        
        of file
        
         imu.c
        
        .
       
References ICM20648_deInit() , and IMU_STATE_DISABLED .
Referenced by IMU_gyroCalibrate() .
| void IMU_fuseAccelerometerSetSampleRate | ( | IMU_SensorFusion * | 
            f,
            | 
| float | 
            rate
            | ||
| ) | 
Sets the accelerometer sample rate in the IMU_SensorFusion structure.
Sensor Fusion functions
- Parameters
- 
         [out] fPointer to the IMU_SensorFusion object [in] rateSample rate of the accelerometer 
- Returns
- None
        Definition at line
        
         117
        
        of file
        
         imu_fuse.c
        
        .
       
References _IMU_SensorFusion::gSampleRate .
Referenced by IMU_config() .
| void IMU_fuseAccelerometerUpdateFilter | ( | IMU_SensorFusion * | 
            f,
            | 
| float | 
            avec[3]
            | ||
| ) | 
The current accelerometer data is added to the accumulator.
- Parameters
- 
         [out] fPointer to the IMU_SensorFusion object [in] avecAccelerometer vector 
- Returns
- None
        Definition at line
        
         137
        
        of file
        
         imu_fuse.c
        
        .
       
References _IMU_SensorFusion::aAccumulator , and _IMU_SensorFusion::aAccumulatorCount .
Referenced by IMU_fuseUpdate() .
| void IMU_fuseGyroCorrection | ( | IMU_SensorFusion * | 
            f,
            | 
| bool | 
            accValid,
            | ||
| bool | 
            dirValid,
            | ||
| float | 
            dirZ
            | ||
| ) | 
Calculates the gyro correction vector.
- Parameters
- 
         [out] fPointer to the IMU_SensorFusion object [in] accValidTrue if the acceration value is within the limits [in] dirValidTrue if the direction value is valid [in] dirZThe direction of the Z axis 
- Returns
- None
        Definition at line
        
         216
        
        of file
        
         imu_fuse.c
        
        .
       
References _IMU_SensorFusion::angleCorrection , _IMU_SensorFusion::aVector , _IMU_SensorFusion::gSampleRate , IMU_vectorNormalizeAngle() , IMU_vectorScale() , IMU_vectorSubtract() , IMU_vectorZero() , and _IMU_SensorFusion::orientation .
Referenced by IMU_fuseUpdate() .
| void IMU_fuseGyroCorrectionClear | ( | IMU_SensorFusion * | 
            f
            | ) | 
Clears the gyro correction vector.
- Parameters
- 
         [out] fPointer to the IMU_SensorFusion object 
- Returns
- None
        Definition at line
        
         158
        
        of file
        
         imu_fuse.c
        
        .
       
References _IMU_SensorFusion::angleCorrection , and IMU_vectorZero() .
| void IMU_fuseGyroSetSampleRate | ( | IMU_SensorFusion * | 
            f,
            | 
| float | 
            rate
            | ||
| ) | 
Sets the gyro sample rate and related values in the IMU_SensorFusion structure.
- Parameters
- 
         [out] fPointer to the IMU_SensorFusion object [in] rateSample rate of the gyroscope 
- Returns
- None
        Definition at line
        
         95
        
        of file
        
         imu_fuse.c
        
        .
       
References _IMU_SensorFusion::gDeltaTime , _IMU_SensorFusion::gDeltaTimeScale , and _IMU_SensorFusion::gSampleRate .
Referenced by IMU_config() .
| void IMU_fuseGyroUpdate | ( | IMU_SensorFusion * | 
            f,
            | 
| float | 
            gvec[3]
            | ||
| ) | 
Updates the fusion calculation with a new gyro data.
- Parameters
- 
         [out] fPointer to the IMU_SensorFusion object [in] gvecGyroscope vector 
- Returns
- None
        Definition at line
        
         178
        
        of file
        
         imu_fuse.c
        
        .
       
References _IMU_SensorFusion::angleCorrection , _IMU_SensorFusion::dcm , _IMU_SensorFusion::gDeltaTimeScale , IMU_dcmGetAngles() , IMU_dcmNormalize() , IMU_dcmRotate() , IMU_vectorAdd() , IMU_vectorScalarMultiplication() , and _IMU_SensorFusion::orientation .
Referenced by IMU_fuseUpdate() .
| void IMU_fuseNew | ( | IMU_SensorFusion * | 
            f
            | ) | 
Initializes a new IMU_SensorFusion structure.
- Parameters
- 
         [out] fPointer to the IMU_SensorFusion object to be initialized 
- Returns
- None
        Definition at line
        
         48
        
        of file
        
         imu_fuse.c
        
        .
       
References _IMU_SensorFusion::aAccumulator , _IMU_SensorFusion::aAccumulatorCount , _IMU_SensorFusion::angleCorrection , _IMU_SensorFusion::aSampleRate , _IMU_SensorFusion::aVector , _IMU_SensorFusion::dcm , _IMU_SensorFusion::gDeltaTime , _IMU_SensorFusion::gSampleRate , _IMU_SensorFusion::gVector , and _IMU_SensorFusion::orientation .
Referenced by IMU_init() .
| void IMU_fuseReset | ( | IMU_SensorFusion * | 
            f
            | ) | 
Clears the values of the sensor fusion object.
- Parameters
- 
         [out] fPointer to the IMU_SensorFusion object 
- Returns
- None
        Definition at line
        
         301
        
        of file
        
         imu_fuse.c
        
        .
       
References _IMU_SensorFusion::aAccumulator , _IMU_SensorFusion::aAccumulatorCount , _IMU_SensorFusion::angleCorrection , _IMU_SensorFusion::aVector , _IMU_SensorFusion::dcm , _IMU_SensorFusion::gVector , IMU_dcmReset() , IMU_vectorZero() , and _IMU_SensorFusion::orientation .
Referenced by IMU_config() , and IMU_reset() .
| void IMU_fuseUpdate | ( | IMU_SensorFusion * | 
            f
            | ) | 
Updates the fusion calculation.
- Parameters
- 
         [out] fPointer to the IMU_SensorFusion object 
- Returns
- None
        Definition at line
        
         325
        
        of file
        
         imu_fuse.c
        
        .
       
References _IMU_SensorFusion::aVector , _IMU_SensorFusion::gVector , IMU_fuseAccelerometerUpdateFilter() , IMU_fuseGyroCorrection() , IMU_fuseGyroUpdate() , IMU_getAccelerometerData() , IMU_getGyroData() , and IMU_STATE_READY .
Referenced by IMU_update() .
| void IMU_getAccelerometerData | ( | float | 
            avec[3]
            | ) | 
Retrieves the raw acceleration data from the IMU.
- Parameters
- 
         [out] avecThree dimensonal raw acceleration vector 
- Returns
- None
        Definition at line
        
         351
        
        of file
        
         imu.c
        
        .
       
References ICM20648_accelDataRead() , and IMU_STATE_READY .
Referenced by IMU_fuseUpdate() .
| void IMU_getGyroCorrectionAngles | ( | float | 
            acorr[3]
            | ) | 
Retrieves the processed gyroscope correction angles.
- Parameters
- 
         [out] acorrThree dimensonal gyro correction angle vector 
- Returns
- None
        Definition at line
        
         375
        
        of file
        
         imu.c
        
        .
       
References _IMU_SensorFusion::angleCorrection .
| void IMU_getGyroData | ( | float | 
            gvec[3]
            | ) | 
Retrieves the raw gyroscope data from the IMU.
- Parameters
- 
         [out] gvecThree dimensonal raw gyro vector 
- Returns
- None
        Definition at line
        
         394
        
        of file
        
         imu.c
        
        .
       
References ICM20648_gyroDataRead() , and IMU_STATE_READY .
Referenced by IMU_fuseUpdate() .
| uint8_t IMU_getState | ( | void | 
            | ) | 
Returns IMU state.
- Returns
- Returns zero on OK, non-zero otherwise
        Definition at line
        
         150
        
        of file
        
         imu.c
        
        .
       
| uint32_t IMU_gyroCalibrate | ( | void | 
            | ) | 
Performs gyroscope calibration to cancel gyro bias.
- Returns
- None
        Definition at line
        
         294
        
        of file
        
         imu.c
        
        .
       
References ICM20648_interruptEnable() , IMU_config() , IMU_deInit() , IMU_init() , and IMU_OK .
| void IMU_gyroGet | ( | int16_t | 
            gvec[3]
            | ) | 
Retrieves the processed gyroscope data.
- Parameters
- 
         [out] gvecThree dimensonal gyro vector 
- Returns
- None
        Definition at line
        
         278
        
        of file
        
         imu.c
        
        .
       
References _IMU_SensorFusion::gVector .
| uint32_t IMU_init | ( | void | 
            | ) | 
Initializes and calibrates the IMU.
- Returns
- Returns zero on OK, non-zero otherwise
Module functions
        Definition at line
        
         74
        
        of file
        
         imu.c
        
        .
       
References GPIOINT_Init() , ICM20648_deInit() , ICM20648_getDeviceID() , ICM20648_gyroCalibrate() , ICM20648_init() , ICM20648_OK , IMU_fuseNew() , IMU_STATE_CALIBRATING , IMU_STATE_DISABLED , and IMU_STATE_INITIALIZING .
Referenced by IMU_gyroCalibrate() .
| bool IMU_isDataReady | ( | void | 
            | ) | 
Checks if there is new accel/gyro data available for read.
- Returns
- True if the measurement data is ready, false otherwise
        Definition at line
        
         415
        
        of file
        
         imu.c
        
        .
       
References ICM20648_isDataReady() , and IMU_STATE_READY .
| bool IMU_isDataReadyFlag | ( | void | 
            | ) | 
Checks if there is new accel/gyro data available for read. In case of ver 0.3.0 and older of the PIC firmware the state of the PIC_INT_WAKE needs to be read to determinte if the IMU interrupt is valid.
- Returns
- True if data ready flag is set, false otherwise
        Definition at line
        
         443
        
        of file
        
         imu.c
        
        .
       
References IMU_STATE_READY .
| void IMU_matrixMultiply | ( | float | 
            c[3][3],
            | 
| float | 
            a[3][3],
            | ||
| float | 
            b[3][3]
            | ||
| ) | 
Multiplies two 3x3 matrices.
- Parameters
- 
         [out] cThe multiplication result, AB [in] aInput vector A [in] bInput vector B 
- Returns
- None
        Definition at line
        
         67
        
        of file
        
         imu_math.c
        
        .
       
Referenced by IMU_dcmRotate() .
| void IMU_normalizeAngle | ( | float * | 
            a
            | ) | 
Normalizes the angle ( -PI < angle <= PI )
Vector and Matrix math
- Parameters
- 
         aThe angle to be normalized 
- Returns
- None
        Definition at line
        
         38
        
        of file
        
         imu_math.c
        
        .
       
Referenced by IMU_vectorNormalizeAngle() .
| void IMU_orientationGet | ( | int16_t | 
            ovec[3]
            | ) | 
Retrieves the processed orientation data.
- Parameters
- 
         [out] ovecThree dimensonal orientation vector 
- Returns
- None
        Definition at line
        
         259
        
        of file
        
         imu.c
        
        .
       
References _IMU_SensorFusion::orientation .
| void IMU_reset | ( | void | 
            | ) | 
Resets the fusion calculation.
- Returns
- None
        Definition at line
        
         334
        
        of file
        
         imu.c
        
        .
       
References IMU_fuseReset() .
| void IMU_update | ( | void | 
            | ) | 
Gets a new set of data from the accel and gyro sensor and updates the fusion calculation.
- Returns
- None
        Definition at line
        
         320
        
        of file
        
         imu.c
        
        .
       
References IMU_fuseUpdate() .
| void IMU_vectorAdd | ( | float | 
            r[3],
            | 
| float | 
            a[3],
            | ||
| float | 
            b[3]
            | ||
| ) | 
Adds two vectors.
- Parameters
- 
         [out] rThe vectorial sum of the vectors, a+b [in] aThe first vector [in] bThe second vector 
- Returns
- None
        Definition at line
        
         193
        
        of file
        
         imu_math.c
        
        .
       
Referenced by IMU_dcmNormalize() , and IMU_fuseGyroUpdate() .
| void IMU_vectorCrossProduct | ( | float | 
            r[3],
            | 
| float | 
            a[3],
            | ||
| float | 
            b[3]
            | ||
| ) | 
Calculates the cross product of two vectors.
- Parameters
- 
         [out] rThe cross product [in] aThe first vector [in] bThe second vector 
- Returns
- None
        Definition at line
        
         273
        
        of file
        
         imu_math.c
        
        .
       
Referenced by IMU_dcmNormalize() , and IMU_dcmResetZ() .
| float IMU_vectorDotProduct | ( | float | 
            a[3],
            | 
| float | 
            b[3]
            | ||
| ) | 
Calculates the dot product of two vectors.
- Parameters
- 
         [in] aThe first vector [in] bThe second vector 
- Returns
- The dot product
        Definition at line
        
         244
        
        of file
        
         imu_math.c
        
        .
       
Referenced by IMU_dcmNormalize() .
| void IMU_vectorNormalizeAngle | ( | float | 
            v[3]
            | ) | 
Normalizes the angle of a vector.
- Parameters
- 
         vThe vector, which contains angles to be normalized 
- Returns
- None
        Definition at line
        
         94
        
        of file
        
         imu_math.c
        
        .
       
References IMU_normalizeAngle() .
Referenced by IMU_fuseGyroCorrection() .
| void IMU_vectorScalarMultiplication | ( | float | 
            r[3],
            | 
| float | 
            v[3],
            | ||
| float | 
            scale
            | ||
| ) | 
Multiplies a vector by a scalar.
- Parameters
- 
         [out] rThe multiplied vector [in] vThe vector to be multiplied [in] scaleThe scalar multiplicator value 
- Returns
- None
        Definition at line
        
         142
        
        of file
        
         imu_math.c
        
        .
       
Referenced by IMU_dcmNormalize() , and IMU_fuseGyroUpdate() .
| void IMU_vectorScale | ( | float | 
            v[3],
            | 
| float | 
            scale
            | ||
| ) | 
Scales a vector by a factor.
- Parameters
- 
         vThe vector to be scaled [in] scaleThe scale factor 
- Returns
- None
        Definition at line
        
         166
        
        of file
        
         imu_math.c
        
        .
       
Referenced by IMU_dcmResetZ() , and IMU_fuseGyroCorrection() .
| void IMU_vectorSubtract | ( | float | 
            r[3],
            | 
| float | 
            a[3],
            | ||
| float | 
            b[3]
            | ||
| ) | 
Subtracts vector b from vector a.
- Parameters
- 
         [out] rThe vectorial difference, a-b [in] aVector a [in] bVector b 
- Returns
- None
        Definition at line
        
         220
        
        of file
        
         imu_math.c
        
        .
       
Referenced by IMU_fuseGyroCorrection() .
| void IMU_vectorZero | ( | float | 
            v[3]
            | ) | 
Sets all elements of a vector to 0.
- Parameters
- 
         vThe vector to be cleared 
- Returns
- None
        Definition at line
        
         115
        
        of file
        
         imu_math.c
        
        .
       
Referenced by IMU_fuseGyroCorrection() , IMU_fuseGyroCorrectionClear() , and IMU_fuseReset() .