MSDSCSI_ReadCapacity_TypeDef Struct ReferenceKit Drivers > Gecko USB MSD

SCSI Read Capacity Command Descriptor Block (CDB) typedef.

Definition at line 177 of file msdscsi.h.

#include <msdscsi.h>

Data Fields

struct {
   uint8_t   Obsolete: 1
 
   uint8_t   Reserved1: 7
 
}; 
 
struct {
   uint8_t   Pmi: 1
 
   uint8_t   Reserved3: 7
 
}; 
 
uint8_t Control
 
uint32_t Lba
 
uint8_t OpCode
 
uint16_t Reserved2
 

Field Documentation

uint8_t MSDSCSI_ReadCapacity_TypeDef::Control

Control byte.

Definition at line 189 of file msdscsi.h.

uint32_t MSDSCSI_ReadCapacity_TypeDef::Lba

Logical Block (sector) Address.

Definition at line 183 of file msdscsi.h.

uint8_t MSDSCSI_ReadCapacity_TypeDef::Obsolete

Obsolete, expect any value.

Definition at line 180 of file msdscsi.h.

uint8_t MSDSCSI_ReadCapacity_TypeDef::OpCode

Command opcode.

Definition at line 178 of file msdscsi.h.

uint8_t MSDSCSI_ReadCapacity_TypeDef::Pmi

Partial medium indicator.

Definition at line 186 of file msdscsi.h.

uint8_t MSDSCSI_ReadCapacity_TypeDef::Reserved1

Reserved, expect 0.

Definition at line 181 of file msdscsi.h.

uint16_t MSDSCSI_ReadCapacity_TypeDef::Reserved2

Reserved, expect 0.

Definition at line 184 of file msdscsi.h.

uint8_t MSDSCSI_ReadCapacity_TypeDef::Reserved3

Reserved, expect 0.

Definition at line 187 of file msdscsi.h.


The documentation for this struct was generated from the following file:
  • C:/cygwin/home/caamunds/work/super/hardware/kit/common/drivers/msdscsi.h