SE_Command_t Struct ReferenceEMLIB > SE
SE Command structure to which all commands to the SE must adhere.
       Definition at line
       
        325
       
       of file
       
        em_se.h
       
       .
      
      
       #include <
       
     
        em_se.h
       
       >
      
| Data Fields | |
| uint32_t | command | 
| SE_DataTransfer_t * | data_in | 
| SE_DataTransfer_t * | data_out | 
| size_t | num_parameters | 
| uint32_t | parameters [ SE_MAX_PARAMETERS ] | 
The documentation for this struct was generated from the following file:
- 
       C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
       em_se.h