DISPLAY_Device_t Struct ReferenceKit Drivers > Display
Display device data structure, including a specification of how the display device behaves.
       Definition at line
       
        100
       
       of file
       
        display.h
       
       .
      
      
       #include <
       
     
        display.h
       
       >
      
| Data Fields | |
| DISPLAY_AddressMode_t | addressMode | 
| DISPLAY_ColourMode_t | colourMode | 
| DISPLAY_Geometry_t | geometry | 
| char * | name | 
| EMSTATUS(* | pDisplayPowerOn )(struct DISPLAY_Device_t *device, bool on) | 
| EMSTATUS(* | pDriverRefresh )(struct DISPLAY_Device_t *device) | 
| EMSTATUS(* | pPixelMatrixAllocate )(struct DISPLAY_Device_t *device, unsigned int width, unsigned int height, DISPLAY_PixelMatrix_t *pixelMatrix) | 
| EMSTATUS(* | pPixelMatrixClear )(struct DISPLAY_Device_t *device, DISPLAY_PixelMatrix_t pixelMatrix, unsigned int width, unsigned int height) | 
| EMSTATUS(* | pPixelMatrixDraw )(struct DISPLAY_Device_t *device, DISPLAY_PixelMatrix_t pixelMatrix, unsigned int startColumn, unsigned int width, unsigned int startRow, unsigned int height) | 
| EMSTATUS(* | pPixelMatrixFree )(struct DISPLAY_Device_t *device, DISPLAY_PixelMatrix_t pixelMatrix) | 
Field Documentation
| DISPLAY_AddressMode_t DISPLAY_Device_t::addressMode | 
Address mode of the display device.
        Definition at line
        
         104
        
        of file
        
         display.h
        
        .
       
| DISPLAY_ColourMode_t DISPLAY_Device_t::colourMode | 
Colour mode of the display device.
        Definition at line
        
         103
        
        of file
        
         display.h
        
        .
       
| DISPLAY_Geometry_t DISPLAY_Device_t::geometry | 
Geometry of the display device.
        Definition at line
        
         102
        
        of file
        
         display.h
        
        .
       
| char* DISPLAY_Device_t::name | 
Name of the display device.
        Definition at line
        
         101
        
        of file
        
         display.h
        
        .
       
| EMSTATUS(* DISPLAY_Device_t::pDisplayPowerOn) (struct DISPLAY_Device_t *device, bool on) | 
Turn power on display on or off.
        Definition at line
        
         107
        
        of file
        
         display.h
        
        .
       
| EMSTATUS(* DISPLAY_Device_t::pDriverRefresh) (struct DISPLAY_Device_t *device) | 
Refreshes the display device driver after system change, like changing a clock frequency of some related device.
        Definition at line
        
         146
        
        of file
        
         display.h
        
        .
       
Referenced by DISPLAY_DriverRefresh() .
| EMSTATUS(* DISPLAY_Device_t::pPixelMatrixAllocate) (struct DISPLAY_Device_t *device, unsigned int width, unsigned int height, DISPLAY_PixelMatrix_t *pixelMatrix) | 
Allocates a pixelMatrix buffer in the format specified by the geometry ( DISPLAY_Geometry_t ) of the display device.
        Definition at line
        
         112
        
        of file
        
         display.h
        
        .
       
| EMSTATUS(* DISPLAY_Device_t::pPixelMatrixClear) (struct DISPLAY_Device_t *device, DISPLAY_PixelMatrix_t pixelMatrix, unsigned int width, unsigned int height) | 
Clears a pixelMatrix buffer by setting all pixels to black.
        Definition at line
        
         138
        
        of file
        
         display.h
        
        .
       
| EMSTATUS(* DISPLAY_Device_t::pPixelMatrixDraw) (struct DISPLAY_Device_t *device, DISPLAY_PixelMatrix_t pixelMatrix, unsigned int startColumn, unsigned int width, unsigned int startRow, unsigned int height) | 
Copies the contents of the specified pixelMatrix buffer to the display device.
        Definition at line
        
         127
        
        of file
        
         display.h
        
        .
       
| EMSTATUS(* DISPLAY_Device_t::pPixelMatrixFree) (struct DISPLAY_Device_t *device, DISPLAY_PixelMatrix_t pixelMatrix) | 
Frees a pixelMatrix buffer
        Definition at line
        
         122
        
        of file
        
         display.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/cygwin/home/caamunds/work/super/hardware/kit/common/drivers/
       display.h