BURTCEMLIB
Detailed Description
Backup Real Time Counter (BURTC) Peripheral API.
This module contains functions to control the BURTC peripheral of Silicon Labs 32-bit MCUs. The Backup Real Time Counter allows timekeeping in all energy modes. The Backup RTC is also available when the system is in backup mode.
| Data Structures | |
| struct | BURTC_Init_TypeDef | 
| Macros | |
| #define | BURTC_INIT_DEFAULT | 
| #define | burtcClkDiv_1 1 | 
| #define | burtcClkDiv_128 128 | 
| #define | burtcClkDiv_16 16 | 
| #define | burtcClkDiv_2 2 | 
| #define | burtcClkDiv_32 32 | 
| #define | burtcClkDiv_4 4 | 
| #define | burtcClkDiv_64 64 | 
| #define | burtcClkDiv_8 8 | 
| Functions | |
| uint32_t | BURTC_ClockFreqGet (void) | 
| uint32_t | BURTC_CompareGet (unsigned int comp) | 
| Get the BURTC compare value. | |
| void | BURTC_CompareSet (unsigned int comp, uint32_t value) | 
| Set BURTC compare channel. | |
| __STATIC_INLINE uint32_t | BURTC_CounterGet (void) | 
| Get BURTC counter. | |
| void | BURTC_CounterReset (void) | 
| Reset counter. | |
| void | BURTC_Enable (bool enable) | 
| Enable or Disable BURTC peripheral. | |
| void | BURTC_Init (const BURTC_Init_TypeDef *burtcInit) | 
| Initialize BURTC. | |
| __STATIC_INLINE void | BURTC_IntClear (uint32_t flags) | 
| Clear one or more pending BURTC interrupts. | |
| __STATIC_INLINE void | BURTC_IntDisable (uint32_t flags) | 
| Disable one or more BURTC interrupts. | |
| __STATIC_INLINE void | BURTC_IntEnable (uint32_t flags) | 
| Enable one or more BURTC interrupts. | |
| __STATIC_INLINE uint32_t | BURTC_IntGet (void) | 
| Get pending BURTC interrupt flags. | |
| __STATIC_INLINE uint32_t | BURTC_IntGetEnabled (void) | 
| Get enabled and pending BURTC interrupt flags. | |
| __STATIC_INLINE void | BURTC_IntSet (uint32_t flags) | 
| Set one or more pending BURTC interrupts from SW. | |
| __STATIC_INLINE void | BURTC_Lock (void) | 
| Lock BURTC registers, will protect from writing new config settings. | |
| void | BURTC_Reset (void) | 
| Restore BURTC to reset state. | |
| __STATIC_INLINE void | BURTC_Start (void) | 
| Start BURTC counter. | |
| __STATIC_INLINE uint32_t | BURTC_Status (void) | 
| Status of BURTC RAM, timestamp and LP Mode. | |
| __STATIC_INLINE void | BURTC_Stop (void) | 
| Stop the BURTC counter. | |
| __STATIC_INLINE void | BURTC_SyncWait (void) | 
| Wait for the BURTC to complete all synchronization of register changes and commands. | |
| __STATIC_INLINE void | BURTC_Unlock (void) | 
| Unlock BURTC registers, enable write access to change configuration. | |
Macro Definition Documentation
| #define BURTC_INIT_DEFAULT | 
Default configuration for BURTC init structure
        Definition at line
        
         155
        
        of file
        
         em_burtc.h
        
        .
       
| #define burtcClkDiv_1 1 | 
BURTC clock divisors. These values are valid for the BURTC prescaler. Divide clock by 1.
        Definition at line
        
         60
        
        of file
        
         em_burtc.h
        
        .
       
| #define burtcClkDiv_128 128 | 
Divide clock by 128.
        Definition at line
        
         67
        
        of file
        
         em_burtc.h
        
        .
       
| #define burtcClkDiv_16 16 | 
Divide clock by 16.
        Definition at line
        
         64
        
        of file
        
         em_burtc.h
        
        .
       
| #define burtcClkDiv_2 2 | 
Divide clock by 2.
        Definition at line
        
         61
        
        of file
        
         em_burtc.h
        
        .
       
| #define burtcClkDiv_32 32 | 
Divide clock by 32.
        Definition at line
        
         65
        
        of file
        
         em_burtc.h
        
        .
       
| #define burtcClkDiv_4 4 | 
Divide clock by 4.
        Definition at line
        
         62
        
        of file
        
         em_burtc.h
        
        .
       
| #define burtcClkDiv_64 64 | 
Divide clock by 64.
        Definition at line
        
         66
        
        of file
        
         em_burtc.h
        
        .
       
| #define burtcClkDiv_8 8 | 
Divide clock by 8.
        Definition at line
        
         63
        
        of file
        
         em_burtc.h
        
        .
       
Function Documentation
| uint32_t BURTC_CompareGet | ( | unsigned int | 
            comp
            | ) | 
Get the BURTC compare value.
- Parameters
- 
         [in] compCompare the channel index value, must be 0 for Giant/Leopard Gecko. 
- Returns
- The currently configured value for this compare channel.
        Definition at line
        
         300
        
        of file
        
         em_burtc.c
        
        .
       
| void BURTC_CompareSet | ( | unsigned int | 
            comp,
            | 
| uint32_t | 
            value
            | ||
| ) | 
Set BURTC compare channel.
- Parameters
- 
         [in] compCompare the channel index, must be 0 for current devices. [in] valueNew compare value. 
        Definition at line
        
         270
        
        of file
        
         em_burtc.c
        
        .
       
| __STATIC_INLINE uint32_t BURTC_CounterGet | ( | void | 
            | ) | 
Get BURTC counter.
- Returns
- BURTC counter value
        Definition at line
        
         372
        
        of file
        
         em_burtc.h
        
        .
       
| void BURTC_Enable | ( | bool | 
            enable
            | ) | 
Enable or Disable BURTC peripheral.
- Parameters
- 
         [in] enabletrue to enable, false to disable. 
        Definition at line
        
         223
        
        of file
        
         em_burtc.c
        
        .
       
References BURTC_Stop() , and BURTC_SyncWait() .
Referenced by BURTC_Init() .
| void BURTC_Init | ( | const BURTC_Init_TypeDef * | 
            burtcInit
            | ) | 
Initialize BURTC.
Configures the BURTC peripheral.
- Note
- 
         Before initialization, BURTC module must first be enabled by clearing the reset bit in the RMU, i.e.,
         * RMU_ResetControl(rmuResetBU, rmuResetModeClear); * Compare channel 0 must be configured outside this function, before initialization if enable is set to true. The counter will always be reset.
- Parameters
- 
         [in] burtcInitA pointer to the BURTC initialization structure. 
        Definition at line
        
         128
        
        of file
        
         em_burtc.c
        
        .
       
References BURTC_Enable() , BURTC_IntClear() , BURTC_Start() , BURTC_SyncWait() , BURTC_Init_TypeDef::clkDiv , BURTC_Init_TypeDef::compare0Top , BURTC_Init_TypeDef::debugRun , BURTC_Init_TypeDef::em4comp , BURTC_Init_TypeDef::em4overflow , and BURTC_Init_TypeDef::start .
| __STATIC_INLINE void BURTC_IntClear | ( | uint32_t | 
            flags
            | ) | 
Clear one or more pending BURTC interrupts.
- Parameters
- 
         [in] flagsBURTC interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources for the BURTC module (BURTC_IFS_nnn). 
        Definition at line
        
         179
        
        of file
        
         em_burtc.h
        
        .
       
Referenced by BURTC_Init() .
| __STATIC_INLINE void BURTC_IntDisable | ( | uint32_t | 
            flags
            | ) | 
Disable one or more BURTC interrupts.
- Parameters
- 
         [in] flagsBURTC interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt sources for the BURTC module (BURTC_IFS_nnn). 
        Definition at line
        
         197
        
        of file
        
         em_burtc.h
        
        .
       
| __STATIC_INLINE void BURTC_IntEnable | ( | uint32_t | 
            flags
            | ) | 
Enable one or more BURTC interrupts.
- Note
- Depending on use, a pending interrupt may already be set prior to enabling the interrupt. Consider using BURTC_IntClear() prior to enabling if a pending interrupt should be ignored.
- Parameters
- 
         [in] flagsBURTC interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the BURTC module (BURTC_IFS_nnn). 
        Definition at line
        
         220
        
        of file
        
         em_burtc.h
        
        .
       
| __STATIC_INLINE uint32_t BURTC_IntGet | ( | void | 
            | ) | 
Get pending BURTC interrupt flags.
- Note
- This function does not clear the event bits.
- Returns
- Pending BURTC interrupt sources. Returns a set of interrupt flags OR-ed together for multiple interrupt sources in the BURTC module (BURTC_IFS_nnn).
        Definition at line
        
         240
        
        of file
        
         em_burtc.h
        
        .
       
| __STATIC_INLINE uint32_t BURTC_IntGetEnabled | ( | void | 
            | ) | 
Get enabled and pending BURTC interrupt flags.
- Note
- The event bits are not cleared by the use of this function.
- Returns
- Pending BURTC interrupt sources that is also enabled. Returns a set of interrupt flags OR-ed together for multiple interrupt sources in the BURTC module (BURTC_IFS_nnn).
        Definition at line
        
         257
        
        of file
        
         em_burtc.h
        
        .
       
| __STATIC_INLINE void BURTC_IntSet | ( | uint32_t | 
            flags
            | ) | 
Set one or more pending BURTC interrupts from SW.
- Parameters
- 
         [in] flagsBURTC interrupt sources to set to pending. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the BURTC module (BURTC_IFS_nnn). 
        Definition at line
        
         277
        
        of file
        
         em_burtc.h
        
        .
       
| void BURTC_Reset | ( | void | 
            | ) | 
Restore BURTC to reset state.
- Note
- Before accessing the BURTC, BURSTEN in RMU->CTRL must be cleared. LOCK will not be reset to default value, as this will disable access to core BURTC registers.
        Definition at line
        
         336
        
        of file
        
         em_burtc.c
        
        .
       
References BURTC_Stop() , BURTC_SyncWait() , BUS_RegBitRead() , and BUS_RegBitWrite() .
| __STATIC_INLINE void BURTC_Start | ( | void | 
            | ) | 
Start BURTC counter.
This function will send a start command to the BURTC peripheral. The BURTC peripheral will use some LF clock ticks before the command is executed. The BURTC_SyncWait() function can be used to wait for the start command to be executed.
- Note
- This function requires the BURTC to be enabled.
        Definition at line
        
         340
        
        of file
        
         em_burtc.h
        
        .
       
References BURTC_SyncWait() .
Referenced by BURTC_CounterReset() , and BURTC_Init() .
| __STATIC_INLINE uint32_t BURTC_Status | ( | void | 
            | ) | 
Status of BURTC RAM, timestamp and LP Mode.
- Returns
- A mask logially OR-ed status bits
        Definition at line
        
         292
        
        of file
        
         em_burtc.h
        
        .
       
| __STATIC_INLINE void BURTC_Stop | ( | void | 
            | ) | 
Stop the BURTC counter.
This function will send a stop command to the BURTC peripheral. The BURTC peripheral will use some LF clock ticks before the command is executed. The BURTC_SyncWait() function can be used to wait for the stop command to be executed.
- Note
- This function requires the BURTC to be enabled.
        Definition at line
        
         359
        
        of file
        
         em_burtc.h
        
        .
       
References BURTC_SyncWait() .
Referenced by BURTC_CounterReset() , BURTC_Enable() , and BURTC_Reset() .