IADC_Result_t Struct ReferenceEMLIB > IADC
Structure holding IADC result, including data and ID
       Definition at line
       
        813
       
       of file
       
        em_iadc.h
       
       .
      
      
       #include <
       
     
        em_iadc.h
       
       >
      
| Data Fields | |
| uint32_t | data | 
| uint8_t | id | 
Field Documentation
| uint32_t IADC_Result_t::data | 
ADC sample data.
        Definition at line
        
         814
        
        of file
        
         em_iadc.h
        
        .
       
| uint8_t IADC_Result_t::id | 
Id of FIFO entry; Scan table entry id or single indicator (0x20).
        Definition at line
        
         815
        
        of file
        
         em_iadc.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/super/platform/emlib/inc/
       em_iadc.h