SE_OTPInit_t Struct ReferenceEMLIB > SE
       Definition at line
       
        351
       
       of file
       
        em_se.h
       
       .
      
| Data Fields | |
| bool | enableAntiRollback | 
| bool | enableSecureBoot | 
| bool | secureBootPageLockFull | 
| bool | secureBootPageLockNarrow | 
| bool | verifySecureBootCertificate | 
Field Documentation
| bool SE_OTPInit_t::enableAntiRollback | 
Enable anti-rollback for host application upgrades.
        Definition at line
        
         357
        
        of file
        
         em_se.h
        
        .
       
| bool SE_OTPInit_t::enableSecureBoot | 
Enable secure boot for the host.
        Definition at line
        
         353
        
        of file
        
         em_se.h
        
        .
       
| bool SE_OTPInit_t::secureBootPageLockFull | 
Set flag to enable locking down all flash pages that cover the secure-booted image, including the last page if end of signature is not page-aligned.
        Definition at line
        
         366
        
        of file
        
         em_se.h
        
        .
       
| bool SE_OTPInit_t::secureBootPageLockNarrow | 
Set flag to enable locking down all flash pages that cover the secure-booted image, except the last page if end of signature is not page-aligned.
        Definition at line
        
         362
        
        of file
        
         em_se.h
        
        .
       
| bool SE_OTPInit_t::verifySecureBootCertificate | 
Require certificate based secure boot signing.
        Definition at line
        
         355
        
        of file
        
         em_se.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/super/platform/emlib/inc/
       em_se.h