IADC_Config_t Struct ReferenceEMLIB > IADC
IADC config structure
       Definition at line
       
        661
       
       of file
       
        em_iadc.h
       
       .
      
      
       #include <
       
     
        em_iadc.h
       
       >
      
Field Documentation
| uint8_t IADC_Config_t::adcClkPrescale | 
ADC_CLK divider (prescale+1).
        Definition at line
        
         667
        
        of file
        
         em_iadc.h
        
        .
       
Referenced by IADC_init() .
| IADC_CfgAdcMode_t IADC_Config_t::adcMode | 
IADC mode; Normal, High speed or High Accuracy.
        Definition at line
        
         662
        
        of file
        
         em_iadc.h
        
        .
       
Referenced by IADC_init() .
| IADC_CfgAnalogGain_t IADC_Config_t::analogGain | 
| IADC_CfgOsrHighSpeed_t IADC_Config_t::osrHighSpeed | 
Over sampling ratio for High Speed and Normal modes.
        Definition at line
        
         663
        
        of file
        
         em_iadc.h
        
        .
       
Referenced by IADC_init() .
| IADC_CfgReference_t IADC_Config_t::reference | 
| IADC_CfgTwosComp_t IADC_Config_t::twosComplement | 
| uint32_t IADC_Config_t::vRef | 
Vref magnitude expressed in millivolts.
        Definition at line
        
         668
        
        of file
        
         em_iadc.h
        
        .
       
Referenced by IADC_init() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/super/platform/emlib/inc/
       em_iadc.h