LETIMEREMLIB
Detailed Description
Low Energy Timer (LETIMER) Peripheral API.
This module contains functions to control the LETIMER peripheral of Silicon Labs 32-bit MCUs and SoCs. The LETIMER is a down-counter that can keep track of time and output configurable waveforms.
| Data Structures | |
| struct | LETIMER_Init_TypeDef | 
| Macros | |
| #define | LETIMER_INIT_DEFAULT | 
| Enumerations | |
| enum | LETIMER_RepeatMode_TypeDef
         
         { letimerRepeatFree = _LETIMER_CTRL_REPMODE_FREE, letimerRepeatOneshot = _LETIMER_CTRL_REPMODE_ONESHOT, letimerRepeatBuffered = _LETIMER_CTRL_REPMODE_BUFFERED, letimerRepeatDouble = _LETIMER_CTRL_REPMODE_DOUBLE } | 
| enum | LETIMER_UFOA_TypeDef
         
         { letimerUFOANone = _LETIMER_CTRL_UFOA0_NONE, letimerUFOAToggle = _LETIMER_CTRL_UFOA0_TOGGLE, letimerUFOAPulse = _LETIMER_CTRL_UFOA0_PULSE, letimerUFOAPwm = _LETIMER_CTRL_UFOA0_PWM } | 
| Functions | |
| uint32_t | LETIMER_CompareGet (LETIMER_TypeDef *letimer, unsigned int comp) | 
| Get the LETIMER compare register value. | |
| void | LETIMER_CompareSet (LETIMER_TypeDef *letimer, unsigned int comp, uint32_t value) | 
| Set the LETIMER compare register value. | |
| uint32_t | LETIMER_CounterGet (LETIMER_TypeDef *letimer) | 
| Get LETIMER counter value. | |
| void | LETIMER_CounterSet (LETIMER_TypeDef *letimer, uint32_t value) | 
| Set LETIMER counter value. | |
| void | LETIMER_Enable (LETIMER_TypeDef *letimer, bool enable) | 
| Start/stop LETIMER. | |
| void | LETIMER_Init (LETIMER_TypeDef *letimer, const LETIMER_Init_TypeDef *init) | 
| Initialize LETIMER. | |
| __STATIC_INLINE void | LETIMER_IntClear (LETIMER_TypeDef *letimer, uint32_t flags) | 
| Clear one or more pending LETIMER interrupts. | |
| __STATIC_INLINE void | LETIMER_IntDisable (LETIMER_TypeDef *letimer, uint32_t flags) | 
| Disable one or more LETIMER interrupts. | |
| __STATIC_INLINE void | LETIMER_IntEnable (LETIMER_TypeDef *letimer, uint32_t flags) | 
| Enable one or more LETIMER interrupts. | |
| __STATIC_INLINE uint32_t | LETIMER_IntGet (LETIMER_TypeDef *letimer) | 
| Get pending LETIMER interrupt flags. | |
| __STATIC_INLINE uint32_t | LETIMER_IntGetEnabled (LETIMER_TypeDef *letimer) | 
| Get enabled and pending LETIMER interrupt flags. | |
| __STATIC_INLINE void | LETIMER_IntSet (LETIMER_TypeDef *letimer, uint32_t flags) | 
| Set one or more pending LETIMER interrupts from SW. | |
| uint32_t | LETIMER_RepeatGet (LETIMER_TypeDef *letimer, unsigned int rep) | 
| Get the LETIMER repeat register value. | |
| void | LETIMER_RepeatSet (LETIMER_TypeDef *letimer, unsigned int rep, uint32_t value) | 
| Set the LETIMER repeat counter register value. | |
| void | LETIMER_Reset (LETIMER_TypeDef *letimer) | 
| Reset LETIMER to the same state that it was in after a hardware reset. | |
| void | LETIMER_SyncWait (LETIMER_TypeDef *letimer) | 
| Wait for the LETIMER to complete all synchronization of register changes and commands. | |
| uint32_t | LETIMER_TopGet (LETIMER_TypeDef *letimer) | 
| Get the current LETIMER top value. | |
| void | LETIMER_TopSet (LETIMER_TypeDef *letimer, uint32_t value) | 
| Set the LETIMER top value. | |
Macro Definition Documentation
| #define LETIMER_INIT_DEFAULT | 
Default configuration for LETIMER initialization structure.
        Definition at line
        
         126
        
        of file
        
         em_letimer.h
        
        .
       
Referenced by MIC_init() .
Enumeration Type Documentation
Repeat mode.
        Definition at line
        
         57
        
        of file
        
         em_letimer.h
        
        .
       
| enum LETIMER_UFOA_TypeDef | 
Underflow action on output.
        Definition at line
        
         75
        
        of file
        
         em_letimer.h
        
        .
       
Function Documentation
| uint32_t LETIMER_CompareGet | ( | LETIMER_TypeDef * | 
            letimer,
            | 
| unsigned int | 
            comp
            | ||
| ) | 
Get the LETIMER compare register value.
- Parameters
- 
         [in] letimerA pointer to the LETIMER peripheral register block. [in] compA compare register to get, either 0 or 1. 
- Returns
- A compare register value, 0 if invalid register selected.
        Definition at line
        
         129
        
        of file
        
         em_letimer.c
        
        .
       
| void LETIMER_CompareSet | ( | LETIMER_TypeDef * | 
            letimer,
            | 
| unsigned int | 
            comp,
            | ||
| uint32_t | 
            value
            | ||
| ) | 
Set the LETIMER compare register value.
- Note
- The setting of a compare register requires synchronization into the low frequency domain. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the LETIMER_Sync() internal function call.
- Parameters
- 
         [in] letimerA pointer to the LETIMER peripheral register block. [in] compA compare register to set, either 0 or 1. [in] valueAn initialization value (<= 0x0000ffff). 
        Definition at line
        
         218
        
        of file
        
         em_letimer.c
        
        .
       
Referenced by LETIMER_TopSet() , and MIC_init() .
| uint32_t LETIMER_CounterGet | ( | LETIMER_TypeDef * | 
            letimer
            | ) | 
Get LETIMER counter value.
- Parameters
- 
         [in] letimerPointer to the LETIMER peripheral register block. 
- Returns
- Current LETIMER counter value.
        Definition at line
        
         170
        
        of file
        
         em_letimer.c
        
        .
       
| void LETIMER_CounterSet | ( | LETIMER_TypeDef * | 
            letimer,
            | 
| uint32_t | 
            value
            | ||
| ) | 
Set LETIMER counter value.
- Parameters
- 
         [in] letimerPointer to the LETIMER peripheral register block. [in] valueNew counter value. 
        Definition at line
        
         189
        
        of file
        
         em_letimer.c
        
        .
       
| void LETIMER_Enable | ( | LETIMER_TypeDef * | 
            letimer,
            | 
| bool | 
            enable
            | ||
| ) | 
Start/stop LETIMER.
- Note
- The enabling/disabling of the LETIMER modifies the LETIMER CMD register which requires synchronization into the low-frequency domain. If this register is modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the LETIMER_Sync() internal function call.
- Parameters
- 
         [in] letimerA pointer to the LETIMER peripheral register block. [in] enableTrue to enable counting, false to disable. 
        Definition at line
        
         272
        
        of file
        
         em_letimer.c
        
        .
       
| void LETIMER_Init | ( | LETIMER_TypeDef * | 
            letimer,
            | 
| const LETIMER_Init_TypeDef * | 
            init
            | ||
| ) | 
Initialize LETIMER.
Note that the compare/repeat values must be set separately with LETIMER_CompareSet() and LETIMER_RepeatSet() . That should probably be done prior using this function if configuring the LETIMER to start when initialization is complete.
- Note
- The initialization of the LETIMER modifies the LETIMER CTRL/CMD registers which require synchronization into the low-frequency domain. If any of those registers are modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the LETIMER_Sync() internal function call.
- Parameters
- 
         [in] letimerA pointer to the LETIMER peripheral register block. [in] initA pointer to the LETIMER initialization structure. 
        Definition at line
        
         363
        
        of file
        
         em_letimer.c
        
        .
       
References LETIMER_Init_TypeDef::bufTop , LETIMER_Init_TypeDef::comp0Top , LETIMER_Init_TypeDef::debugRun , LETIMER_Init_TypeDef::enable , LETIMER_Init_TypeDef::out0Pol , LETIMER_Init_TypeDef::out1Pol , LETIMER_Init_TypeDef::repMode , LETIMER_Init_TypeDef::topValue , LETIMER_Init_TypeDef::ufoa0 , and LETIMER_Init_TypeDef::ufoa1 .
Referenced by MIC_init() .
| __STATIC_INLINE void LETIMER_IntClear | ( | LETIMER_TypeDef * | 
            letimer,
            | 
| uint32_t | 
            flags
            | ||
| ) | 
Clear one or more pending LETIMER interrupts.
- Parameters
- 
         [in] letimerPointer to LETIMER peripheral register block. [in] flagsPending LETIMER interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn). 
        Definition at line
        
         172
        
        of file
        
         em_letimer.h
        
        .
       
Referenced by LETIMER_Reset() .
| __STATIC_INLINE void LETIMER_IntDisable | ( | LETIMER_TypeDef * | 
            letimer,
            | 
| uint32_t | 
            flags
            | ||
| ) | 
Disable one or more LETIMER interrupts.
- Parameters
- 
         [in] letimerPointer to LETIMER peripheral register block. [in] flagsLETIMER interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn). 
        Definition at line
        
         192
        
        of file
        
         em_letimer.h
        
        .
       
| __STATIC_INLINE void LETIMER_IntEnable | ( | LETIMER_TypeDef * | 
            letimer,
            | 
| uint32_t | 
            flags
            | ||
| ) | 
Enable one or more LETIMER interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using LETIMER_IntClear() prior to enabling the interrupt.
- Parameters
- 
         [in] letimerPointer to the LETIMER peripheral register block. [in] flagsLETIMER interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn). 
        Definition at line
        
         213
        
        of file
        
         em_letimer.h
        
        .
       
| __STATIC_INLINE uint32_t LETIMER_IntGet | ( | LETIMER_TypeDef * | 
            letimer
            | ) | 
Get pending LETIMER interrupt flags.
- Note
- Event bits are not cleared by the use of this function.
- Parameters
- 
         [in] letimerPointer to LETIMER peripheral register block. 
- Returns
- LETIMER interrupt sources pending. A bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn).
        Definition at line
        
         232
        
        of file
        
         em_letimer.h
        
        .
       
| __STATIC_INLINE uint32_t LETIMER_IntGetEnabled | ( | LETIMER_TypeDef * | 
            letimer
            | ) | 
Get enabled and pending LETIMER interrupt flags.
Useful for handling more interrupt sources in the same interrupt handler.
- Note
- Event bits are not cleared by the use of this function.
- Parameters
- 
         [in] letimerPointer to LETIMER peripheral register block. 
- Returns
- 
         Pending and enabled LETIMER interrupt sources. Return value is the bitwise AND combination of
         - the OR combination of enabled interrupt sources in LETIMER_IEN_nnn register (LETIMER_IEN_nnn) and
- the OR combination of valid interrupt flags of the LETIMER module (LETIMER_IF_nnn).
 
        Definition at line
        
         258
        
        of file
        
         em_letimer.h
        
        .
       
| __STATIC_INLINE void LETIMER_IntSet | ( | LETIMER_TypeDef * | 
            letimer,
            | 
| uint32_t | 
            flags
            | ||
| ) | 
Set one or more pending LETIMER interrupts from SW.
- Parameters
- 
         [in] letimerPointer to LETIMER peripheral register block. [in] flagsLETIMER interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for the LETIMER module (LETIMER_IF_nnn). 
        Definition at line
        
         281
        
        of file
        
         em_letimer.h
        
        .
       
| uint32_t LETIMER_RepeatGet | ( | LETIMER_TypeDef * | 
            letimer,
            | 
| unsigned int | 
            rep
            | ||
| ) | 
Get the LETIMER repeat register value.
- Parameters
- 
         [in] letimerA pointer to the LETIMER peripheral register block. [in] repRepeat register to get, either 0 or 1. 
- Returns
- Repeat register value, 0 if invalid register selected.
        Definition at line
        
         459
        
        of file
        
         em_letimer.c
        
        .
       
| void LETIMER_RepeatSet | ( | LETIMER_TypeDef * | 
            letimer,
            | 
| unsigned int | 
            rep,
            | ||
| uint32_t | 
            value
            | ||
| ) | 
Set the LETIMER repeat counter register value.
- Note
- The setting of a repeat counter register requires synchronization into the low-frequency domain. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the LETIMER_Sync() internal function call.
- Parameters
- 
         [in] letimerA pointer to the LETIMER peripheral register block. [in] repRepeat counter register to set, either 0 or 1. [in] valueAn initialization value (<= 0x0000ffff). 
        Definition at line
        
         511
        
        of file
        
         em_letimer.c
        
        .
       
Referenced by MIC_init() .
| void LETIMER_Reset | ( | LETIMER_TypeDef * | 
            letimer
            | ) | 
Reset LETIMER to the same state that it was in after a hardware reset.
- Note
- The ROUTE register is NOT reset by this function to allow for a centralized setup of this feature.
- Parameters
- 
         [in] letimerA pointer to the LETIMER peripheral register block. 
        Definition at line
        
         557
        
        of file
        
         em_letimer.c
        
        .
       
References LETIMER_IntClear() , and LETIMER_SyncWait() .
| uint32_t LETIMER_TopGet | ( | LETIMER_TypeDef * | 
            letimer
            | ) | 
Get the current LETIMER top value.
- Parameters
- 
         [in] letimerA pointer to the LETIMER peripheral register block. 
- Returns
- The top value. This will be a 16 bit value on series-0 and series-1 devices and a 24 bit value on series-2 devices.
        Definition at line
        
         659
        
        of file
        
         em_letimer.c
        
        .
       
| void LETIMER_TopSet | ( | LETIMER_TypeDef * | 
            letimer,
            | 
| uint32_t | 
            value
            | ||
| ) | 
Set the LETIMER top value.
- Note
- The LETIMER is a down-counter, so when the counter reaches 0 then the top value will be loaded into the counter. This function can be used to set the top value.
If the LETIMER is not already configured to use a top value then this function will enable that functionality for the user.
- Parameters
- 
         [in] letimerA pointer to the LETIMER peripheral register block. [in] valueThe top value. This can be a 16 bit value on series-0 and series-1 devices and a 24 bit value on series-2 devices. 
        Definition at line
        
         625
        
        of file
        
         em_letimer.c
        
        .
       
References LETIMER_CompareSet() .