SLISTPlatform Common
| Data Structures | |
| struct | sl_slist_node | 
| Typedefs | |
| typedef struct sl_slist_node | sl_slist_node_t | 
| Functions | |
| void | sl_slist_init ( sl_slist_node_t **head) | 
| void | sl_slist_insert ( sl_slist_node_t *item, sl_slist_node_t *pos) | 
| sl_slist_node_t * | sl_slist_pop ( sl_slist_node_t **head) | 
| void | sl_slist_push ( sl_slist_node_t **head, sl_slist_node_t *item) | 
| void | sl_slist_push_back ( sl_slist_node_t **head, sl_slist_node_t *item) | 
| void | sl_slist_remove ( sl_slist_node_t **head, sl_slist_node_t *item) | 
| void | sl_slist_sort ( sl_slist_node_t **head, bool(*cmp_fnct)( sl_slist_node_t *item_l, sl_slist_node_t *item_r)) | 
Macro Definition Documentation
| #define SL_SLIST_FOR_EACH_ENTRY | ( | 
            list_head,
            | |
| 
            entry,
            | |||
| 
            type,
            | |||
| 
            member
            | |||
| ) | 
        Definition at line
        
         54
        
        of file
        
         sl_slist.h
        
        .
       
Function Documentation
| void sl_slist_init | ( | sl_slist_node_t ** | 
            head
            | ) | 
Initializes a singly-linked list.
- Parameters
- 
         headPointer to pointer of head element of list. 
Initializes a singly-linked list.
        Definition at line
        
         32
        
        of file
        
         sl_slist.c
        
        .
       
| void sl_slist_insert | ( | sl_slist_node_t * | 
            item,
            | 
| sl_slist_node_t * | 
            pos
            | ||
| ) | 
Insert item after given item.
- Parameters
- 
         itemPointer to item to add. posPointer to item after which the item to add will be inserted. 
Insert item after given item.
        Definition at line
        
         85
        
        of file
        
         sl_slist.c
        
        .
       
| sl_slist_node_t * sl_slist_pop | ( | sl_slist_node_t ** | 
            head
            | ) | 
Removes and returns first element of list.
- Parameters
- 
         headPointer to pointer of head element of list. 
- Returns
- Pointer to item that was at top of the list.
Removes and returns first element of list.
        Definition at line
        
         66
        
        of file
        
         sl_slist.c
        
        .
       
| void sl_slist_push | ( | sl_slist_node_t ** | 
            head,
            | 
| sl_slist_node_t * | 
            item
            | ||
| ) | 
Add given item at beginning of list.
- Parameters
- 
         headPointer to pointer of head element of list. itemPointer to item to add. 
Add given item at beginning of list.
        Definition at line
        
         40
        
        of file
        
         sl_slist.c
        
        .
       
| void sl_slist_push_back | ( | sl_slist_node_t ** | 
            head,
            | 
| sl_slist_node_t * | 
            item
            | ||
| ) | 
Add item at end of list.
- Parameters
- 
         headPointer to pointer of head element of list. itemPointer to item to add. 
Add item at end of list.
        Definition at line
        
         50
        
        of file
        
         sl_slist.c
        
        .
       
| void sl_slist_remove | ( | sl_slist_node_t ** | 
            head,
            | 
| sl_slist_node_t * | 
            item
            | ||
| ) | 
Remove item from list.
- Parameters
- 
         headPointer to pointer of head element of list. itemPointer to item to remove. 
- Note
- (1) An EFM_ASSERT is thrown if the item is not found within the list.
Remove item from list.
        Definition at line
        
         95
        
        of file
        
         sl_slist.c
        
        .
       
| void sl_slist_sort | ( | sl_slist_node_t ** | 
            head,
            | 
| bool(*)( sl_slist_node_t *item_l, sl_slist_node_t *item_r) | 
            cmp_fnct
            | ||
| ) | 
Sorts list items.
- Parameters
- 
         headPointer to pointer of head element of list. cmp_fnctPointer to function to use for sorting the list. item_l Pointer to left item. item_r Pointer to right item. Returns whether the two items are ordered (true) or not (false). 
Sorts list items.
        Definition at line
        
         113
        
        of file
        
         sl_slist.c
        
        .