EZRADIODRV_PacketTxHandle Struct ReferenceEMDRV > EZRADIODRV > Plugin_System > Transmit_Plugin
EzRadio transmit plug-in instance initialization and handler structure.
       Definition at line
       
        98
       
       of file
       
        ezradio_transmit_plugin.h
       
       .
      
      
       #include <
       
     
        ezradio_transmit_plugin.h
       
       >
      
| Data Fields | |
| uint8_t | channel | 
| Transmission channel. | |
| EZRADIODRV_PacketLengthConfig_t | lenConfig | 
| Packet length configuration. | |
| uint16_t | pktId | 
| Packet ID. | |
| EZRADIODRV_TransmitPacketType_t | pktType | 
| Packet type. | |
| EZRADIODRV_Callback_t | userCallback | 
| User callback. | |
The documentation for this struct was generated from the following file:
- 
       C:/repos/super/platform/emdrv/ezradiodrv/plugins/inc/
       ezradio_transmit_plugin.h