EZRADIODRV_AutoAckHandle Struct ReferenceEMDRV > EZRADIODRV > Plugin_System > Auto_ACK_Plugin
EzRadio auto acknowledge plug-in instance initialization and handler structure.
       Definition at line
       
        76
       
       of file
       
        ezradio_auto_ack_plugin.h
       
       .
      
      
       #include <
       
     
        ezradio_auto_ack_plugin.h
       
       >
      
| Data Fields | |
| EZRADIODRV_AutoAckMode_t | ackMode | 
| Auto ack mode. | |
| EZRADIODRV_PacketLengthConfig_t | lenConfig | 
| Pakcet length config for auto ack. | |
| uint8_t * | pktBuf | 
| Pointer to the buffer that holds the auto ack packet. | |
| uint16_t | pktId | 
| Auto ack packet ID. | |
| EZRADIODRV_AutoAckPacketMode_t | pktMode | 
| Packet mode for aut ack. | |
| EZRADIODRV_Callback_t | userCallback | 
| User callback. | |
The documentation for this struct was generated from the following file:
- 
       C:/repos/super/platform/emdrv/ezradiodrv/plugins/inc/
       ezradio_auto_ack_plugin.h