EZRADIODRV_HandleData Struct ReferenceEMDRV > EZRADIODRV > Plugin_System > Plugin_Manager
EzRadio driver instance initialization and handler structure. This data structure contains a number of EzRadio driver configuration options. Handler to this structure is passed to ezradioInit() when initializing an EzRadio driver instance. Some common initialization data sets are predefined in EZRADIODRV_INIT_DEFAULT . Note: All the referenced plug-in instances has there own handler sturcture, that is referenced from this structure.
       Definition at line
       
        299
       
       of file
       
        ezradio_plugin_manager.h
       
       .
      
      
       #include <
       
     
        ezradio_plugin_manager.h
       
       >
      
| Data Fields | |
| EZRADIODRV_AutoAckHandle_t | autoAck | 
| Auto-acknowledge plug-in handler. | |
| EZRADIODRV_DirectRxHandle_t | directRx | 
| Direct reception plug-in handler. | |
| EZRADIODRV_DirectTxHandle_t | directTx | 
| Direct transmission plug-in handler. | |
| EZRADIODRV_PacketCrcErrorHandle_t | packetCrcError | 
| Packet reception with CRC error plug-in handler. | |
| EZRADIODRV_PacketRxHandle_t | packetRx | 
| Packet reception plug-in handler. | |
| EZRADIODRV_PacketTxHandle_t | packetTx | 
| Packet transmission plug-in handler. | |
| EZRADIODRV_Pn9Handle_t | pn9 | 
| PN9 plug-in handler. | |
| EZRADIODRV_UnmodCarrierHandle_t | unmodCarrier | 
| Unmodulated carrier plug-in handler. | |
The documentation for this struct was generated from the following file:
- 
       C:/repos/super/platform/emdrv/ezradiodrv/plugins/inc/
       ezradio_plugin_manager.h