TEXTDISPLAY_Config_t Struct ReferenceKit Drivers > Textdisplay
Initialization data structure for text display devices.
       Definition at line
       
        82
       
       of file
       
        textdisplay.h
       
       .
      
      
       #include <
       
     
        textdisplay.h
       
       >
      
| Data Fields | |
| int | displayDeviceNo | 
| bool | lfToCrLf | 
| bool | scrollEnable | 
Field Documentation
| int TEXTDISPLAY_Config_t::displayDeviceNo | 
Display device number to initialize test display on.
        Definition at line
        
         83
        
        of file
        
         textdisplay.h
        
        .
       
Referenced by RETARGET_TextDisplayInit() , and TEXTDISPLAY_New() .
| bool TEXTDISPLAY_Config_t::lfToCrLf | 
Enable or disable LF to CR+LF conversion.
        Definition at line
        
         90
        
        of file
        
         textdisplay.h
        
        .
       
Referenced by RETARGET_TextDisplayInit() , and TEXTDISPLAY_New() .
| bool TEXTDISPLAY_Config_t::scrollEnable | 
Enable/disable scrolling mode on the text display. Scrolling mode will consume more memory because the lines will have to be stored in memory.
        Definition at line
        
         85
        
        of file
        
         textdisplay.h
        
        .
       
Referenced by RETARGET_TextDisplayInit() , and TEXTDISPLAY_New() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/super/hardware/kit/common/drivers/
       textdisplay.h