UARTDRV_InitUart_t Struct ReferenceEMDRV > UARTDRV
A UART driver instance initialization structure. Contains a number of UARTDRV configuration options. It is required for driver instance initialization. This structure is passed to UARTDRV_Init() when initializing a UARTDRV instance.
       Definition at line
       
        192
       
       of file
       
        uartdrv.h
       
       .
      
      
       #include <
       
     
        uartdrv.h
       
       >
      
| Data Fields | |
| uint32_t | baudRate | 
| UART baud rate. | |
| uint8_t | ctsPin | 
| A CTS pin number. | |
| GPIO_Port_TypeDef | ctsPort | 
| A CTS pin port number. | |
| UARTDRV_FlowControlType_t | fcType | 
| Flow control mode. | |
| bool | mvdis | 
| Majority Vote Disable for 16x, 8x and 6x oversampling modes. | |
| USART_OVS_TypeDef | oversampling | 
| Oversampling mode. | |
| USART_Parity_TypeDef | parity | 
| Parity configuration. | |
| USART_TypeDef * | port | 
| The peripheral used for UART. | |
| uint8_t | rtsPin | 
| An RTS pin number. | |
| GPIO_Port_TypeDef | rtsPort | 
| An RTS pin port number. | |
| uint8_t | rxPin | 
| Pin number for UART Rx. | |
| GPIO_Port_TypeDef | rxPort | 
| Port for UART Rx pin. | |
| UARTDRV_Buffer_FifoQueue_t * | rxQueue | 
| A receive operation queue. | |
| USART_Stopbits_TypeDef | stopBits | 
| A number of stop bits. | |
| uint8_t | txPin | 
| Pin number for UART Tx. | |
| GPIO_Port_TypeDef | txPort | 
| Port for UART Tx pin. | |
| UARTDRV_Buffer_FifoQueue_t * | txQueue | 
| T transmit operation queue. | |
| uint8_t | uartNum | 
| UART instance number. | |
The documentation for this struct was generated from the following file:
- 
       C:/repos/super/platform/emdrv/uartdrv/inc/
       uartdrv.h