INTEMLIB
Detailed Description
Safe nesting of interrupt disable/enable API.
- 
       
        Deprecated:
- These functions are deprecated and marked for removal in a later release. Use the CORE module instead. See Porting from em_int for information on how to convert existing code bases to use CORE .
This module contains functions to safely disable and enable interrupts at the CPU level. INT_Disable() disables interrupts globally and increments a lock level counter (counting semaphore). INT_Enable() decrements the lock level counter and enables interrupts if the counter reaches zero.
These functions would normally be used to secure critical regions and to make sure that a critical section that calls into another critical section does not unintentionally terminate the callee critical section.
These functions should also be used inside interrupt handlers:
*  void SysTick_Handler(void)
*  {
*    INT_Disable();
*      .
*      .
*      .
*    INT_Enable();
*  }
* 
     | Functions | |
| __STATIC_INLINE uint32_t | INT_Disable (void) | 
| Disable interrupts. | |
| __STATIC_INLINE uint32_t | INT_Enable (void) | 
| Enable interrupts. | |
| Variables | |
| uint32_t | INT_LockCnt = 0 | 
Function Documentation
| __STATIC_INLINE uint32_t INT_Disable | ( | void | 
            | ) | 
Disable interrupts.
- 
         
          Deprecated:
- Deprecated and marked for removal in a later release. Use new CORE module instead.
Disable interrupts and increment lock level counter.
- Returns
- Resulting interrupt disable nesting level.
        Definition at line
        
         76
        
        of file
        
         em_int.h
        
        .
       
References INT_LockCnt .
| __STATIC_INLINE uint32_t INT_Enable | ( | void | 
            | ) | 
Enable interrupts.
- 
         
          Deprecated:
- Deprecated and marked for removal in a later release. Use the new CORE module instead.
- Returns
- Resulting interrupt disable nesting level.
Decrement interrupt lock level counter and enable interrupts if counter reached zero.
        Definition at line
        
         102
        
        of file
        
         em_int.h
        
        .
       
References INT_LockCnt .
Variable Documentation
| uint32_t INT_LockCnt = 0 | 
An interrupt lock level counter. Set to zero initially because main is normally entered with interrupts enabled.
        Definition at line
        
         73
        
        of file
        
         em_int.c
        
        .
       
Referenced by INT_Disable() , and INT_Enable() .