Direct_Receive_PluginEMDRV > EZRADIODRV > Plugin_System
Detailed Description
Direct receive plugin, see Plugin System Layer for detailed documentation.
.
Data Structures | |
struct | EZRADIODRV_DirectRxHandle |
EzRadio direct rx plug-in instance initialization and handler structure. | |
Macros | |
#define | EZRADIODRV_DIRECT_RECEIVE_PLUGIN_INIT_DEFAULT |
Configuration data for EzRadio direct rx plug-in. | |
Typedefs | |
typedef struct EZRADIODRV_DirectRxHandle | EZRADIODRV_DirectRxHandle_t |
EzRadio direct rx plug-in instance initialization and handler structure. | |
Functions | |
Ecode_t | ezradioStartDirectReceive (EZRADIODRV_Handle_t radioHandle) |
Starts direct reception with the radio configurations from the radioHandle parameter. | |
Ecode_t | ezradioStopDirectReceive (void) |
Stops direct reception. | |
Macro Definition Documentation
#define EZRADIODRV_DIRECT_RECEIVE_PLUGIN_INIT_DEFAULT |
Value:
{ /* PN9 */ \
0, /* Channel */ \
},
Configuration data for EzRadio direct rx plug-in.
Definition at line 71
of file ezradio_direct_receive_plugin.h
.
Function Documentation
Ecode_t ezradioStartDirectReceive | ( | EZRADIODRV_Handle_t | radioHandle | ) |
Starts direct reception with the radio configurations from the radioHandle parameter.
- Parameters
-
radioHandle
Handler of the EzRadio driver instance where channel configuration is set.
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
Definition at line 54
of file ezradio_direct_receive_plugin.c
.
References EZRADIODRV_DirectRxHandle::channel, EZRADIODRV_HandleData::directRx, ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE, ECODE_EMDRV_EZRADIODRV_OK, ezradio_get_int_status(), and ezradio_start_rx().
Ecode_t ezradioStopDirectReceive | ( | void |
| ) |
Stops direct reception.
- Returns
- ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
Definition at line 79
of file ezradio_direct_receive_plugin.c
.
References ECODE_EMDRV_EZRADIODRV_OK, and ezradio_change_state().