TouchKit Drivers

Detailed Description

Touch panel driver for DK3650, DK3750 and DK3850 Development Kits.

Data Structures

struct  TOUCH_Config_TypeDef
 
struct  TOUCH_Pos_TypeDef
 

Macros

#define ADC_X   adcSingleInpCh1
 
#define ADC_Y   adcSingleInpCh4
 
#define TOUCH_INIT_DEFAULT
 
#define TOUCH_X1_PIN   5
 
#define TOUCH_X1_PORT   gpioPortD
 
#define TOUCH_X2_PIN   4
 
#define TOUCH_X2_PORT   gpioPortD
 
#define TOUCH_Y1_PIN   3
 
#define TOUCH_Y1_PORT   gpioPortD
 
#define TOUCH_Y2_PIN   1
 
#define TOUCH_Y2_PORT   gpioPortD
 

Typedefs

typedef void( TOUCH_Upcall_TypeDef) (TOUCH_Pos_TypeDef *)
 

Enumerations

enum  TOUCH_State_TypeDef {
  TOUCH_INIT,
  TOUCH_CHECK_PRESS,
  TOUCH_MEASURE_X,
  TOUCH_MEASURE_Y
}
 

Functions

void ADC0_IRQHandler (void)
 Interrupt handler is executed with frequency ~28Hz when panel is not pressed and with frequency ~140Hz when panel is pressed - this will give ~50 readings per second.
 
int TOUCH_CalibrationTable (POINT *displayPtr, POINT *screenPtr)
 Set calibration table.
 
void TOUCH_CallUpcall (void)
 Function that calls registered upcall.
 
TOUCH_Pos_TypeDefTOUCH_GetPos (void)
 Returns current touch position and state.
 
void TOUCH_Init (TOUCH_Config_TypeDef *config)
 Initialize touch panel driver.
 
int TOUCH_IsBusy (void)
 Check status of the touch panel.
 
void TOUCH_RecalculatePosition (volatile TOUCH_Pos_TypeDef *pos)
 Convert ADC readings into XY position.
 
void TOUCH_RegisterUpcall (TOUCH_Upcall_TypeDef *new_upcall)
 Register upcall which will be call every position or state change.
 
int TOUCH_StateChanged (void)
 Check if cursor state changed (down or move)
 

Variables

MATRIX calibrationMatrix = { 103800, 2048, -8184704, -384, 102144, -16424640, 287650 }
 

Macro Definition Documentation

#define ADC_X   adcSingleInpCh1

Input channel 1

Definition at line 63 of file touch.c.

Referenced by ADC0_IRQHandler().

#define ADC_Y   adcSingleInpCh4

Input channel 4

Definition at line 64 of file touch.c.

Referenced by ADC0_IRQHandler(), and TOUCH_Init().

#define TOUCH_INIT_DEFAULT
Value:
{ 500000, /* 500kHz sampling frequency */ \
1, /* Ignore moves not greater than 1 pixel */ \
adcOvsRateSel128, /* Oversampling 128 times */ \
}

Initializes Touch default values

Definition at line 76 of file touch.h.

#define TOUCH_X1_PIN   5

Pin 5

Definition at line 68 of file touch.c.

Referenced by ADC0_IRQHandler().

#define TOUCH_X1_PORT   gpioPortD

Port D

Definition at line 67 of file touch.c.

Referenced by ADC0_IRQHandler().

#define TOUCH_X2_PIN   4

Pin 4

Definition at line 70 of file touch.c.

Referenced by ADC0_IRQHandler(), and TOUCH_IsBusy().

#define TOUCH_X2_PORT   gpioPortD

Port D

Definition at line 69 of file touch.c.

Referenced by ADC0_IRQHandler(), and TOUCH_IsBusy().

#define TOUCH_Y1_PIN   3

Pin 3

Definition at line 72 of file touch.c.

Referenced by ADC0_IRQHandler().

#define TOUCH_Y1_PORT   gpioPortD

Port D

Definition at line 71 of file touch.c.

Referenced by ADC0_IRQHandler().

#define TOUCH_Y2_PIN   1

Pin 1

Definition at line 74 of file touch.c.

Referenced by ADC0_IRQHandler().

#define TOUCH_Y2_PORT   gpioPortD

Port D

Definition at line 73 of file touch.c.

Referenced by ADC0_IRQHandler().

Typedef Documentation

typedef void( TOUCH_Upcall_TypeDef) (TOUCH_Pos_TypeDef *)

touch panel upcall type definition

Definition at line 83 of file touch.h.

Enumeration Type Documentation

touch driver states

Definition at line 77 of file touch.c.

Function Documentation

int TOUCH_CalibrationTable ( POINT *  displayPtr,
POINT *  screenPtr 
)

Set calibration table.

Parameters
[in]displayPtrTable of display points
[in]screenPtrTable of adc values reflecting display points
Returns
Returns OK if calibration table is set.

Definition at line 433 of file touch.c.

References calibrationMatrix.

TOUCH_Pos_TypeDef * TOUCH_GetPos ( void  )

Returns current touch position and state.

Returns
Current touch position and state

Definition at line 396 of file touch.c.

References TOUCH_Pos_TypeDef::adcx, TOUCH_Pos_TypeDef::adcy, TOUCH_Pos_TypeDef::pen, TOUCH_Pos_TypeDef::x, and TOUCH_Pos_TypeDef::y.

void TOUCH_Init ( TOUCH_Config_TypeDef config)

Initialize touch panel driver.

Parameters
configDriver configuration data.

Definition at line 364 of file touch.c.

References ADC_Y, BSP_PeripheralAccess(), BSP_TOUCH, CMU_ClockEnable(), TOUCH_Config_TypeDef::frequency, TOUCH_Config_TypeDef::ignore, and TOUCH_Config_TypeDef::oversampling.

int TOUCH_IsBusy ( void  )

Check status of the touch panel.

Returns
0 if panel is idle (not touched).

Definition at line 344 of file touch.c.

References GPIO_PinInGet(), TOUCH_X2_PIN, and TOUCH_X2_PORT.

void TOUCH_RecalculatePosition ( volatile TOUCH_Pos_TypeDef pos)

Convert ADC readings into XY position.

Parameters
[in]posPointer to position structure

Definition at line 185 of file touch.c.

References TOUCH_Pos_TypeDef::adcx, TOUCH_Pos_TypeDef::adcy, calibrationMatrix, TOUCH_Pos_TypeDef::pen, TOUCH_Pos_TypeDef::x, and TOUCH_Pos_TypeDef::y.

Referenced by ADC0_IRQHandler().

void TOUCH_RegisterUpcall ( TOUCH_Upcall_TypeDef new_upcall)

Register upcall which will be call every position or state change.

Parameters
[in]new_upcallPointer to upcall function

Definition at line 416 of file touch.c.

int TOUCH_StateChanged ( void  )

Check if cursor state changed (down or move)

Returns
1 if the cursor state has changed

Definition at line 228 of file touch.c.

References TOUCH_Pos_TypeDef::pen, TOUCH_Pos_TypeDef::x, and TOUCH_Pos_TypeDef::y.

Referenced by ADC0_IRQHandler().

Variable Documentation

MATRIX calibrationMatrix = { 103800, 2048, -8184704, -384, 102144, -16424640, 287650 }

Calibration table

Definition at line 97 of file touch.c.

Referenced by TOUCH_CalibrationTable(), and TOUCH_RecalculatePosition().