__BAP_Config Struct ReferenceBSP > Thunderboard Sense BSP > BAP - Barometric Pressure Sensor

Structure to configure the BMP280 device.

Definition at line 59 of file bap.h.

#include <bap.h>

Data Fields

uint8_t oversampling
 
uint8_t powerMode
 
uint8_t standbyTime
 

Field Documentation

uint8_t __BAP_Config::oversampling

Oversampling value

Definition at line 60 of file bap.h.

Referenced by BAP_config().

uint8_t __BAP_Config::powerMode

SLEEP, FORCED or NORMAL power mode setting

Definition at line 61 of file bap.h.

Referenced by BAP_config().

uint8_t __BAP_Config::standbyTime

Standby time setting

Definition at line 62 of file bap.h.

Referenced by BAP_config().


The documentation for this struct was generated from the following file:
  • C:/repos/super/hardware/kit/common/bsp/thunderboard/bap.h