VddCheckKit Drivers
Detailed Description
VDD Voltage Check using EMLIB Voltage Comparator (VCOMP) API.
Functions | |
void | VDDCHECK_Disable (void) |
VCMP deinitialization routine. | |
void | VDDCHECK_Init (void) |
VCMP initialization routine. | |
bool | VDDCHECK_LowVoltage (float vdd) |
Check if voltage is higher than indicated. | |
Function Documentation
bool VDDCHECK_LowVoltage | ( | float | vdd | ) |
Check if voltage is higher than indicated.
- Parameters
-
vdd
The voltage level to compare against.
- Returns
- Returns true if voltage is lower, false otherwise
Definition at line 81
of file vddcheck.c
.