__BMP_Palette Struct ReferencePlatform Middleware > GLIB

BMP palette structure to hold palette pointer and size.

Definition at line 133 of file bmp.h.

#include <bmp.h>

Data Fields

uint8_t * data
 
uint32_t size
 

Field Documentation

uint8_t* __BMP_Palette::data

Palette data pointer

Definition at line 135 of file bmp.h.

Referenced by BMP_init(), BMP_readRgbData(), BMP_readRgbDataRLE8(), and BMP_reset().

uint32_t __BMP_Palette::size

Size of palette data

Definition at line 137 of file bmp.h.

Referenced by BMP_init(), and BMP_reset().


The documentation for this struct was generated from the following file:
  • C:/repos/super/platform/middleware/glib/glib/bmp.h