BCP_PacketHeader Struct ReferenceBSP > API for STKs and WSTKs

BCP Packet Header definition.

Definition at line 114 of file bsp_bcp.h.

#include <bsp_bcp.h>

Data Fields

uint8_t magic
 
uint8_t payloadLength
 
uint8_t reserved
 
uint8_t type
 

Field Documentation

uint8_t BCP_PacketHeader::magic

Magic - start of packet - must be BSP_BCP_MAGIC

Definition at line 115 of file bsp_bcp.h.

uint8_t BCP_PacketHeader::payloadLength

Length of data segment >=0 and <=BSP_BCP_PACKET_SIZE

Definition at line 117 of file bsp_bcp.h.

uint8_t BCP_PacketHeader::reserved

Reserved for future expansion

Definition at line 118 of file bsp_bcp.h.

uint8_t BCP_PacketHeader::type

Type - packet type

Definition at line 116 of file bsp_bcp.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super/hardware/kit/common/bsp/bsp_bcp.h