MSDSCSI_RequestSenseData_TypeDef Struct ReferenceKit Drivers > Gecko USB MSD
SCSI Request Sense response data typedef.
Definition at line 158
of file msdscsi.h
.
#include <
msdscsi.h
>
Data Fields | |
struct { | |
uint8_t ResponseCode: 7 | |
uint8_t Valid: 1 | |
}; | |
struct { | |
uint8_t Eom: 1 | |
uint8_t FileMark: 1 | |
uint8_t Ili: 1 | |
uint8_t Reserved: 1 | |
uint8_t SenseKey: 4 | |
}; | |
struct { | |
uint8_t SenseKeySpecific1: 7 | |
uint8_t Sksv: 1 | |
}; | |
uint8_t | AdditionalLength |
uint8_t | Asc |
uint8_t | Ascq |
uint32_t | CmdSpecificInfo |
uint8_t | Fruc |
uint32_t | Information |
uint8_t | Obsolete |
uint8_t | SenseKeySpecific2 |
uint8_t | SenseKeySpecific3 |
Field Documentation
uint8_t MSDSCSI_RequestSenseData_TypeDef::AdditionalLength |
Number of additional sense bytes that follow.
Definition at line 172
of file msdscsi.h
.
uint8_t MSDSCSI_RequestSenseData_TypeDef::Asc |
Additional sense code.
Definition at line 174
of file msdscsi.h
.
uint8_t MSDSCSI_RequestSenseData_TypeDef::Ascq |
Additional sense code qualifier.
Definition at line 175
of file msdscsi.h
.
uint32_t MSDSCSI_RequestSenseData_TypeDef::CmdSpecificInfo |
Command specific information field.
Definition at line 173
of file msdscsi.h
.
uint8_t MSDSCSI_RequestSenseData_TypeDef::Eom |
End of medium indicator.
Definition at line 168
of file msdscsi.h
.
uint8_t MSDSCSI_RequestSenseData_TypeDef::FileMark |
Filemark indicator.
Definition at line 169
of file msdscsi.h
.
uint8_t MSDSCSI_RequestSenseData_TypeDef::Fruc |
Field replacable unit code.
Definition at line 176
of file msdscsi.h
.
uint8_t MSDSCSI_RequestSenseData_TypeDef::Ili |
Incorrect length indicator.
Definition at line 167
of file msdscsi.h
.
uint32_t MSDSCSI_RequestSenseData_TypeDef::Information |
Information field.
Definition at line 171
of file msdscsi.h
.
uint8_t MSDSCSI_RequestSenseData_TypeDef::Obsolete |
Obsolete, expect any value.
Definition at line 163
of file msdscsi.h
.
uint8_t MSDSCSI_RequestSenseData_TypeDef::Reserved |
Reserved, expect 0.
Definition at line 166
of file msdscsi.h
.
uint8_t MSDSCSI_RequestSenseData_TypeDef::ResponseCode |
Response code, 0x70 = Current errors.
Definition at line 160
of file msdscsi.h
.
uint8_t MSDSCSI_RequestSenseData_TypeDef::SenseKey |
Generic error information.
Definition at line 165
of file msdscsi.h
.
uint8_t MSDSCSI_RequestSenseData_TypeDef::SenseKeySpecific1 |
Sense key specific field.
Definition at line 178
of file msdscsi.h
.
uint8_t MSDSCSI_RequestSenseData_TypeDef::SenseKeySpecific2 |
Sense key specific field.
Definition at line 181
of file msdscsi.h
.
uint8_t MSDSCSI_RequestSenseData_TypeDef::SenseKeySpecific3 |
Sense key specific field.
Definition at line 182
of file msdscsi.h
.
uint8_t MSDSCSI_RequestSenseData_TypeDef::Sksv |
Sense key specific field qualifier.
Definition at line 179
of file msdscsi.h
.
uint8_t MSDSCSI_RequestSenseData_TypeDef::Valid |
Valid, qualifier for Information field.
Definition at line 161
of file msdscsi.h
.
The documentation for this struct was generated from the following file:
- C:/repos/super/hardware/kit/common/drivers/
msdscsi.h