MSCEMLIB
Detailed Description
Memory System Controller API.
Contains functions to control the MSC, primarily the Flash. Users can perform Flash memory write and erase operations, as well as optimization of the CPU instruction fetch interface for the application. Available instruction fetch features depends on the MCU or SoC family, but features such as instruction pre-fetch, cache, and configurable branch prediction are typically available.
- Note
- Flash wait-state configuration is handled by CMU module. When core clock configuration is changed by a call to functions such as CMU_ClockSelectSet() or CMU_HFRCOBandSet(), then Flash wait-state configuration is also updated.
MSC resets into a safe state. To initialize the instruction interface to recommended settings:
- Note
- The optimal configuration is highly application dependent. Performance benchmarking is supported by most families. See MSC_StartCacheMeasurement() and MSC_GetCacheMeasurement() for more details.
- The flash write and erase runs from RAM on the EFM32G devices. On all other devices the flash write and erase functions run from flash.
- Flash erase may add ms of delay to interrupt latency if executing from Flash.
Flash write and erase operations are supported by MSC_WriteWord(), MSC_ErasePage(), and MSC_MassErase(). Mass erase is supported for MCU and SoC families with larger Flash sizes.
- Note
- MSC_Init() must be called prior to any Flash write or erase operation.
The following steps are necessary to perform a page erase and write:
Deprecated:
- The configuration called EM_MSC_RUN_FROM_FLASH is deprecated. This was previously used for allocating the flash write functions in either flash or RAM. Flash write functions are now placed in flash on all devices except the EFM32G automatically.
Deprecated:
- The function called MSC_WriteWordFast() is deprecated.
Data Structures | |
struct | MSC_EccConfig_TypeDef |
struct | MSC_ExecConfig_TypeDef |
Macros | |
#define | MSC_ECC_BANKS (1) |
#define | MSC_ECCCONFIG_DEFAULT |
#define | MSC_EXECCONFIG_DEFAULT |
#define | MSC_PROGRAM_TIMEOUT 10000000ul |
Timeout used while waiting for Flash to become ready after a write. This number indicates the number of iterations to perform before issuing a timeout. | |
Enumerations | |
enum | MSC_Status_TypeDef { mscReturnOk = 0, mscReturnInvalidAddr = -1, mscReturnLocked = -2, mscReturnTimeOut = -3, mscReturnUnaligned = -4 } |
Functions | |
void | MSC_Deinit (void) |
Turn off MSC flash write enable and lock MSC registers. | |
void | MSC_EccConfigSet (MSC_EccConfig_TypeDef *eccConfig) |
Configure Error Correcting Code (ECC) | |
MSC_RAMFUNC_DECLARATOR MSC_Status_TypeDef | MSC_ErasePage (uint32_t *startAddress) |
Erases a page in flash memory. | |
void | MSC_ExecConfigSet (MSC_ExecConfig_TypeDef *execConfig) |
Set MSC code execution configuration. | |
void | MSC_Init (void) |
Initialize MSC module. Puts MSC hw in a known state. | |
__STATIC_INLINE void | MSC_IntClear (uint32_t flags) |
Clear one or more pending MSC interrupts. | |
__STATIC_INLINE void | MSC_IntDisable (uint32_t flags) |
Disable one or more MSC interrupts. | |
__STATIC_INLINE void | MSC_IntEnable (uint32_t flags) |
Enable one or more MSC interrupts. | |
__STATIC_INLINE uint32_t | MSC_IntGet (void) |
Get pending MSC interrupt flags. | |
__STATIC_INLINE uint32_t | MSC_IntGetEnabled (void) |
Get enabled and pending MSC interrupt flags. Useful for handling more interrupt sources in the same interrupt handler. | |
__STATIC_INLINE void | MSC_IntSet (uint32_t flags) |
Set one or more pending MSC interrupts from SW. | |
SL_RAMFUNC_DECLARATOR MSC_Status_TypeDef | MSC_MassErase (void) |
MSC_RAMFUNC_DECLARATOR MSC_Status_TypeDef | MSC_WriteWord (uint32_t *address, void const *data, uint32_t numBytes) |
Writes data to flash memory. Write data must be aligned to words and contain a number of bytes that is divisable by four. | |
MSC_RAMFUNC_DECLARATOR MSC_Status_TypeDef | MSC_WriteWordFast (uint32_t *address, void const *data, uint32_t numBytes) |
static void | mscEccBankDisable (const MSC_EccBank_Typedef *eccBank) |
Disable ECC for a given memory bank. | |
static void | mscEccBankInit (const MSC_EccBank_Typedef *eccBank, uint32_t dmaChannels[2]) |
Initialize ECC for a given memory bank. | |
static MSC_RAMFUNC_DEFINITION_END void | mscEccReadWriteExistingPio (const MSC_EccBank_Typedef *eccBank) |
Read and write existing values in RAM (for ECC initializaion). | |
Macro Definition Documentation
#define MSC_ECC_BANKS (1) |
EFR32XG21 incorporates 1 memory bank including ECC support.
Definition at line 225
of file em_msc.h
.
Referenced by MSC_EccConfigSet().
#define MSC_ECCCONFIG_DEFAULT |
Default MSC EccConfig initialization
Definition at line 227
of file em_msc.h
.
#define MSC_EXECCONFIG_DEFAULT |
Default MSC ExecConfig initialization
Definition at line 162
of file em_msc.h
.
#define MSC_PROGRAM_TIMEOUT 10000000ul |
Timeout used while waiting for Flash to become ready after a write. This number indicates the number of iterations to perform before issuing a timeout.
- Note
- Timeout is set very large (in the order of 100x longer than necessary). This is to avoid any corner case.
Definition at line 118
of file em_msc.h
.
Enumeration Type Documentation
enum MSC_Status_TypeDef |
Return codes for writing/erasing Flash.
Definition at line 137
of file em_msc.h
.
Function Documentation
void MSC_EccConfigSet | ( | MSC_EccConfig_TypeDef * | eccConfig | ) |
Configure Error Correcting Code (ECC)
This function configures ECC support according to the configuration input parameter. If the user requests enabling ECC for a given RAM bank this function will initialize ECC memory (syndromes) for the bank by reading and writing the existing values in memory. I.e. all data is preserved. The initialization process runs in a critical section disallowing interrupts and thread scheduling, and will consume a considerable amount of clock cycles. Therefore the user should carefully assess where to call this function. The user can consider to increase the clock frequency in order to reduce the execution time. This function makes use of 2 DMA channels to move data to/from RAM in an efficient way. The user can select which 2 DMA channels to use in order to avoid conflicts with the application. However the user must make sure that no other DMA operations takes place while this function is executing. If the application has been using the DMA controller prior to calling this function, the application will need to reinitialize DMA registers after this function has completed.
- Note
- This function protects the ECC initialization procedure from interrupts and other threads by using a critical section (defined by
em_core.h
) When running on RTOS the user may need to override CORE_EnterCritical CORE_ExitCritical which are declared as 'SL_WEAK' in em_core.c.
- Parameters
-
[in] eccConfig
ECC configuration
Definition at line 1505
of file em_msc.c
.
References MSC_EccConfig_TypeDef::dmaChannels, MSC_EccConfig_TypeDef::enableEccBank, MSC_ECC_BANKS, mscEccBankDisable(), and mscEccBankInit().
MSC_RAMFUNC_DEFINITION_BEGIN MSC_Status_TypeDef MSC_ErasePage | ( | uint32_t * | startAddress | ) |
Erases a page in flash memory.
For IAR Embedded Workbench, Simplicity Studio and GCC this will be achieved automatically by using attributes in the function proctype. For Keil uVision you must define a section called "ram_code" and place this manually in your project's scatter file.
- Parameters
-
[in] startAddress
Pointer to the flash page to erase. Must be aligned to beginning of page boundary.
- Returns
- Returns the status of erase operation, MSC_Status_TypeDef
* mscReturnOk - Operation completed successfully. * mscReturnInvalidAddr - Operation tried to erase a non-flash area. * flashReturnLocked - MSC registers are locked or the operation tried to * erase a locked area of the flash. * flashReturnTimeOut - Operation timed out. *
Definition at line 436
of file em_msc.c
.
References mscReturnOk.
Referenced by NVMHAL_PageErase().
void MSC_ExecConfigSet | ( | MSC_ExecConfig_TypeDef * | execConfig | ) |
Set MSC code execution configuration.
- Parameters
-
[in] execConfig
Code execution configuration
Definition at line 400
of file em_msc.c
.
References MSC_ExecConfig_TypeDef::doutBufEn.
__STATIC_INLINE void MSC_IntClear | ( | uint32_t | flags | ) |
Clear one or more pending MSC interrupts.
- Parameters
-
[in] flags
Pending MSC intterupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the MSC module (MSC_IF_nnn).
Definition at line 262
of file em_msc.h
.
__STATIC_INLINE void MSC_IntDisable | ( | uint32_t | flags | ) |
Disable one or more MSC interrupts.
- Parameters
-
[in] flags
MSC interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the MSC module (MSC_IF_nnn).
Definition at line 279
of file em_msc.h
.
__STATIC_INLINE void MSC_IntEnable | ( | uint32_t | flags | ) |
Enable one or more MSC interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using MSC_IntClear() prior to enabling the interrupt.
- Parameters
-
[in] flags
MSC interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the MSC module (MSC_IF_nnn).
Definition at line 301
of file em_msc.h
.
__STATIC_INLINE uint32_t MSC_IntGet | ( | void |
| ) |
Get pending MSC interrupt flags.
- Note
- The event bits are not cleared by the use of this function.
- Returns
- MSC interrupt sources pending. A bitwise logic OR combination of valid interrupt flags for the MSC module (MSC_IF_nnn).
Definition at line 321
of file em_msc.h
.
__STATIC_INLINE uint32_t MSC_IntGetEnabled | ( | void |
| ) |
Get enabled and pending MSC interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
- Note
- Interrupt flags are not cleared by the use of this function.
- Returns
- Pending and enabled MSC interrupt sources. The return value is the bitwise AND of
- the enabled interrupt sources in MSC_IEN and
- the pending interrupt flags MSC_IF
Definition at line 340
of file em_msc.h
.
__STATIC_INLINE void MSC_IntSet | ( | uint32_t | flags | ) |
Set one or more pending MSC interrupts from SW.
- Parameters
-
[in] flags
MSC interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for the MSC module (MSC_IF_nnn).
Definition at line 356
of file em_msc.h
.
MSC_RAMFUNC_DEFINITION_END MSC_RAMFUNC_DEFINITION_BEGIN MSC_Status_TypeDef MSC_WriteWord | ( | uint32_t * | address, |
void const * | data, |
||
uint32_t | numBytes |
||
) |
Writes data to flash memory. Write data must be aligned to words and contain a number of bytes that is divisable by four.
- Note
- It is recommended to erase the flash page before performing a write.
For IAR Embedded Workbench, Simplicity Studio and GCC this will be achieved automatically by using attributes in the function proctype. For Keil uVision you must define a section called "ram_code" and place this manually in your project's scatter file.
- Parameters
-
[in] address
Pointer to the flash word to write to. Must be aligned to words. [in] data
Data to write to flash. [in] numBytes
Number of bytes to write to flash. NB: Must be divisable by four.
- Returns
- Returns the status of the write operation, MSC_Status_TypeDef
* flashReturnOk - Operation completed successfully. * flashReturnInvalidAddr - Operation tried to write to a non-flash area. * flashReturnLocked - MSC registers are locked or the operation tried to * program a locked area of the flash. * flashReturnTimeOut - Operation timed out. *
Definition at line 494
of file em_msc.c
.
References mscReturnOk, and SL_MIN.
Referenced by NVMHAL_Write().
|
static |
Disable ECC for a given memory bank.
This function disables ECC for a given memory bank which is specified with the MSC_EccBank_Typedef structure input parameter.
- Parameters
-
[in] eccBank
ECC memory bank device structure.
Definition at line 1468
of file em_msc.c
.
Referenced by MSC_EccConfigSet().
|
static |
Initialize ECC for a given memory bank.
This function initializes ECC for a given memory bank which is specified with the MSC_EccBank_Typedef structure input parameter.
- Parameters
-
[in] eccBank
ECC memory bank device structure. [in] dmaChannels
Array of 2 DMA channels that may be used during ECC initialization.
Definition at line 1420
of file em_msc.c
.
References CORE_DECLARE_IRQ_STATE, CORE_ENTER_CRITICAL, CORE_EXIT_CRITICAL, and mscEccReadWriteExistingPio().
Referenced by MSC_EccConfigSet().
|
static |
Read and write existing values in RAM (for ECC initializaion).
This function uses core to load and store the existing data values in the given RAM bank.
- Parameters
-
[in] eccBank
Pointer to ECC RAM bank (MSC_EccBank_Typedef)
Definition at line 1241
of file em_msc.c
.
Referenced by mscEccBankInit().