SE_Command_t Struct ReferenceEMLIB > SE

SE Command structure to which all commands to the SE must adhere.

Definition at line 330 of file em_se.h.

#include <em_se.h>

Data Fields

uint32_t command
 
SE_DataTransfer_tdata_in
 
SE_DataTransfer_tdata_out
 
size_t num_parameters
 
uint32_t parameters [SE_MAX_PARAMETERS]
 

The documentation for this struct was generated from the following file:
  • C:/repos/super/platform/emlib/inc/em_se.h