HIDKBD_Init_t Struct ReferenceKit Drivers > HidKeyboard

HidKeyboard driver initialization structure. This data structure contains configuration options that the driver needs. The structure must be passed to HIDKBD_Init() when initializing the driver.

Definition at line 79 of file hidkbd.h.

#include <hidkbd.h>

Data Fields

void * hidDescriptor
 
HIDKBD_SetReportFunc_t setReportFunc
 

Field Documentation

void* HIDKBD_Init_t::hidDescriptor

Pointer to the HID class descriptor in the user application.

Definition at line 80 of file hidkbd.h.

Referenced by HIDKBD_Init().

HIDKBD_SetReportFunc_t HIDKBD_Init_t::setReportFunc

Callback function pointer for HID output reports, may be NULL when no callback is needed.

Definition at line 81 of file hidkbd.h.

Referenced by HIDKBD_Init().


The documentation for this struct was generated from the following file:
  • C:/repos/super/hardware/kit/common/drivers/hidkbd.h