root_OutputMailbox_t Struct ReferenceEMLIB > SE

Definition at line 98 of file em_se.c.

Data Fields

volatile uint32_t command
 
volatile uint32_t data [0]
 
volatile uint32_t length
 
volatile uint32_t magic
 
volatile uint32_t status
 
volatile uint32_t version
 

The documentation for this struct was generated from the following file:
  • C:/repos/super/platform/emlib/src/em_se.c