__GLIB_Font_t Struct ReferencePlatform Middleware > GLIB
Font definition structure.
Definition at line 224
of file glib.h
.
#include <
glib.h
>
Data Fields | |
uint8_t | charSpacing |
GLIB_Font_Class | class |
uint16_t | cntOfMapElements |
uint8_t | fontHeight |
uint8_t | fontRowOffset |
uint8_t | fontWidth |
uint8_t | lineSpacing |
void * | pFontPixMap |
uint8_t | sizeOfMapElement |
Field Documentation
uint8_t __GLIB_Font_t::charSpacing |
Number of pixels between each character in this font.
Definition at line 247
of file glib.h
.
Referenced by GLIB_drawChar(), and GLIB_drawString().
GLIB_Font_Class __GLIB_Font_t::class |
The font class is used to tell glib if the font contains numbers only or characters and numbers
Definition at line 251
of file glib.h
.
Referenced by GLIB_drawChar(), and GLIB_drawString().
uint16_t __GLIB_Font_t::cntOfMapElements |
Number of elements in the font pixel map.
Definition at line 229
of file glib.h
.
Referenced by GLIB_drawChar().
uint8_t __GLIB_Font_t::fontHeight |
Height in pixels of each character.
Definition at line 241
of file glib.h
.
Referenced by GLIB_drawChar(), and GLIB_drawString().
uint8_t __GLIB_Font_t::fontRowOffset |
uint8_t __GLIB_Font_t::fontWidth |
Width in pixels of each character.
Definition at line 238
of file glib.h
.
Referenced by GLIB_drawChar(), and GLIB_drawString().
uint8_t __GLIB_Font_t::lineSpacing |
Number of pixels between each line in this font.
Definition at line 244
of file glib.h
.
Referenced by GLIB_drawString().
void* __GLIB_Font_t::pFontPixMap |
Pointer to the pixel map for the font.
Definition at line 226
of file glib.h
.
Referenced by GLIB_drawChar().
uint8_t __GLIB_Font_t::sizeOfMapElement |
Size of each element in the font pixel map.
Definition at line 232
of file glib.h
.
Referenced by GLIB_drawChar().
The documentation for this struct was generated from the following file:
- C:/repos/super/platform/middleware/glib/glib/
glib.h