RAIL_BLE_AoxConfig_t Struct Reference
Contains arguments for RAIL_BLE_ConfigAox function.
#include <
rail_ble.h
>
Data Fields | |
RAIL_BLE_AoxOptions_t | aoxOptions |
See RAIL_BLE_AOX_OPTIONS_* for bitfield defines for different AoX features. | |
uint16_t | cteBuffSize |
Size of the raw AoX CTE (continuous tone extension) data capture buffer in bytes. | |
uint32_t * | cteBuffAddr |
Address to where the received CTE is written. | |
uint32_t * | antArrayAddr |
Address to first element of antenna pattern array. | |
uint8_t | antArraySize |
Size of the antenna pattern array. |
Contains arguments for RAIL_BLE_ConfigAox function.
Definition at line 460
of file rail_ble.h
.
The documentation for this struct was generated from the following file:
- protocol/ble/
rail_ble.h