RAIL_MultiTimer_t Struct Reference
RAIL timer state structure.
#include <
rail_types.h
>
Data Fields | |
RAIL_Time_t | absOffset |
Absolute time before the next event. | |
RAIL_Time_t | relPeriodic |
Relative, periodic time between events; 0 = timer is oneshot. | |
RAIL_MultiTimerCallback_t | callback |
A user callback. | |
void * | cbArg |
A user callback argument. | |
struct RAIL_MultiTimer * | next |
A pointer to the next soft timer structure. | |
uint8_t | priority |
A priority of the callback; 0 = highest priority; 255 = lowest. | |
bool | isRunning |
Indicates the timer is currently running. | |
bool | doCallback |
Indicates the callback needs to run. |
RAIL timer state structure.
This structure is filled out and maintained internally only. The user/application should not alter any elements of this structure.
Definition at line 225
of file rail_types.h
.
Field Documentation
◆ absOffset
RAIL_Time_t RAIL_MultiTimer_t::absOffset |
Absolute time before the next event.
Definition at line 226
of file rail_types.h
.
◆ callback
RAIL_MultiTimerCallback_t RAIL_MultiTimer_t::callback |
A user callback.
Definition at line 228
of file rail_types.h
.
◆ cbArg
void* RAIL_MultiTimer_t::cbArg |
A user callback argument.
Definition at line 229
of file rail_types.h
.
◆ doCallback
bool RAIL_MultiTimer_t::doCallback |
Indicates the callback needs to run.
Definition at line 233
of file rail_types.h
.
◆ isRunning
bool RAIL_MultiTimer_t::isRunning |
Indicates the timer is currently running.
Definition at line 232
of file rail_types.h
.
◆ next
struct RAIL_MultiTimer* RAIL_MultiTimer_t::next |
A pointer to the next soft timer structure.
Definition at line 230
of file rail_types.h
.
◆ priority
uint8_t RAIL_MultiTimer_t::priority |
A priority of the callback; 0 = highest priority; 255 = lowest.
Definition at line 231
of file rail_types.h
.
◆ relPeriodic
RAIL_Time_t RAIL_MultiTimer_t::relPeriodic |
Relative, periodic time between events; 0 = timer is oneshot.
Definition at line 227
of file rail_types.h
.
The documentation for this struct was generated from the following file:
- common/
rail_types.h