RAIL_RxChannelHoppingConfigEntry_t Struct Reference
Structure that represents one of the channels that is part of a RAIL_RxChannelHoppingConfig_t sequence of channels used in channel hopping.
#include <
rail_types.h
>
Data Fields |
|
| uint16_t | channel |
|
The channel number to be used for this entry in the channel hopping sequence.
|
|
| RAIL_RxChannelHoppingMode_t | mode |
|
The mode by which RAIL determines when to hop to the next channel.
|
|
| uint32_t | parameter |
|
Depending on the 'mode' parameter that was specified, this member is used to parameterize that mode.
|
|
| uint32_t | delay |
|
Idle time in microseconds to wait before hopping into the channel indicated by this entry.
|
|
| RAIL_RxChannelHoppingDelayMode_t | delayMode |
|
Indicate how the timing specified in 'delay' should be applied.
|
|
| RAIL_RxChannelHoppingOptions_t | options |
|
Bitmask of various options that can be applied to the current channel hop.
|
|
| int8_t | rssiThresholdDbm |
|
The RSSI threshold (in dBm) below which a hop will occur in any mode when
RAIL_RX_CHANNEL_HOPPING_OPTION_RSSI_THRESHOLD
is specified.
|
|
| uint8_t | reserved2 [1] |
|
Pad bytes reserved for future use and currently ignored.
|
|
Structure that represents one of the channels that is part of a RAIL_RxChannelHoppingConfig_t sequence of channels used in channel hopping.
Definition at line
3379
of file
rail_types.h
.
Field Documentation
◆ channel
| uint16_t RAIL_RxChannelHoppingConfigEntry_t::channel |
The channel number to be used for this entry in the channel hopping sequence.
If this is an invalid channel for the current phy, the call to RAIL_ConfigRxChannelHopping will fail.
Definition at line
3385
of file
rail_types.h
.
◆ mode
| RAIL_RxChannelHoppingMode_t RAIL_RxChannelHoppingConfigEntry_t::mode |
The mode by which RAIL determines when to hop to the next channel.
Definition at line
3387
of file
rail_types.h
.
◆ parameter
| uint32_t RAIL_RxChannelHoppingConfigEntry_t::parameter |
Depending on the 'mode' parameter that was specified, this member is used to parameterize that mode.
See the comments on each value of RAIL_RxChannelHoppingMode_t to learn what to specify here.
Definition at line
3394
of file
rail_types.h
.
The documentation for this struct was generated from the following file:
-
common/
rail_types.h