RAIL_Version_t Struct Reference

Contains RAIL Library Version Information.

#include < rail_types.h >

Data Fields

uint32_t hash
Git hash.
uint8_t major
Major number.
uint8_t minor
Minor number.
uint8_t rev
Revision number.
uint8_t build
Build number.
uint8_t flags
Build flags.
bool multiprotocol
Boolean to indicate whether this is a multiprotocol library or not.

Contains RAIL Library Version Information.

It is filled in by RAIL_GetVersion() .

Definition at line 82 of file rail_types.h .

Field Documentation

multiprotocol

bool RAIL_Version_t::multiprotocol

Boolean to indicate whether this is a multiprotocol library or not.

Definition at line 90 of file rail_types.h .


The documentation for this struct was generated from the following file:
  • common/ rail_types.h