RAIL_RxDutyCycleConfig_t Struct Reference
Structure to configure duty cycled receive mode.
#include <
rail_types.h
>
Data Fields | |
RAIL_RxChannelHoppingMode_t | mode |
The mode by which RAIL determines when to exit RX. | |
uint32_t | parameter |
Depending on the 'mode' parameter that was specified, this member is used to parameterize that mode. | |
uint32_t | delay |
Idle time in microseconds to wait before re-entering RX. | |
RAIL_RxChannelHoppingDelayMode_t | delayMode |
Indicate how the timing specified in 'delay' should be applied. | |
RAIL_RxChannelHoppingOptions_t | options |
Bitmask of various options that can be applied to the current duty cycle operation when the mode is >= RAIL_RX_CHANNEL_HOPPING_MODE_MANUAL_WITH_OPTIONS (ignored otherwise). | |
int8_t | rssiThresholdDbm |
The RSSI threshold (in dBm) below which Rx will end in any mode when RAIL_RX_CHANNEL_HOPPING_OPTION_RSSI_THRESHOLD is specified. | |
uint8_t | reserved2 [1] |
Pad bytes reserved for future use and currently ignored. |
Structure to configure duty cycled receive mode.
Definition at line 3468
of file rail_types.h
.
Field Documentation
◆ mode
RAIL_RxChannelHoppingMode_t RAIL_RxDutyCycleConfig_t::mode |
The mode by which RAIL determines when to exit RX.
Definition at line 3470
of file rail_types.h
.
◆ parameter
uint32_t RAIL_RxDutyCycleConfig_t::parameter |
Depending on the 'mode' parameter that was specified, this member is used to parameterize that mode.
See the comments on each value of RAIL_RxChannelHoppingMode_t to learn what to specify here.
Definition at line 3477
of file rail_types.h
.
The documentation for this struct was generated from the following file:
- common/
rail_types.h