RAIL_BLE_State_t Struct Reference
A state structure for BLE.
#include <
rail_ble.h
>
Data Fields | |
uint32_t | crcInit |
The value used to initialize the CRC algorithm. | |
uint32_t | accessAddress |
The access address used for the connection. | |
uint16_t | channel |
The logical channel used. | |
bool | disableWhitening |
Indicates whether the whitening engine should be off. |
A state structure for BLE.
This structure must be allocated in application global read-write memory that persists for the duration of BLE usage. It cannot be allocated in read-only memory or on the call stack.
Definition at line 204
of file rail_ble.h
.
Field Documentation
◆ accessAddress
uint32_t RAIL_BLE_State_t::accessAddress |
The access address used for the connection.
Definition at line 206
of file rail_ble.h
.
◆ channel
uint16_t RAIL_BLE_State_t::channel |
The logical channel used.
Definition at line 207
of file rail_ble.h
.
◆ crcInit
uint32_t RAIL_BLE_State_t::crcInit |
The value used to initialize the CRC algorithm.
Definition at line 205
of file rail_ble.h
.
◆ disableWhitening
bool RAIL_BLE_State_t::disableWhitening |
Indicates whether the whitening engine should be off.
Definition at line 208
of file rail_ble.h
.
The documentation for this struct was generated from the following file:
- protocol/ble/
rail_ble.h