|
|
|
#define
|
TOKEN_NEXT_ADDRESS
(region, address)
|
|
|
By default, tokens are automatically located after the previous token.
|
|
|
|
The following convenience macros are used to simplify the definition process for commonly specified parameters to the basic TOKEN_DEF macro. Please see
hal/micro/token.h
for a more complete explanation.
|
|
#define
|
DEFINE_BASIC_TOKEN
(name, type, ...)
TOKEN_DEF
(name, CREATOR_##name, 0, 0, type, 1, __VA_ARGS__)
|
|
|
|
#define
|
DEFINE_COUNTER_TOKEN
(name, type, ...)
TOKEN_DEF
(name, CREATOR_##name, 1, 0, type, 1, __VA_ARGS__)
|
|
|
|
#define
|
DEFINE_INDEXED_TOKEN
(name, type, arraysize, ...)
TOKEN_DEF
(name, CREATOR_##name, 0, 1, type, (arraysize), __VA_ARGS__)
|
|
|
|
#define
|
DEFINE_FIXED_BASIC_TOKEN
(name, type, address, ...)
|
|
|
|
#define
|
DEFINE_FIXED_COUNTER_TOKEN
(name, type, address, ...)
|
|
|
|
#define
|
DEFINE_FIXED_INDEXED_TOKEN
(name, type, arraysize, address, ...)
|
|
|
|
#define
|
DEFINE_MFG_TOKEN
(name, type, address, ...)
|
|
|
|
The NVM3 object key is used as a distinct identifier tag for a token stored in NVM3.
Every token must have a defined NVM3 object key and the object key must be unique. The object key defined must be in the following format: NVM3KEY_tokenname
where tokenname is the name of the token without NVM3KEY_ or TOKEN_ prefix.
|
|
#define
|
NVM3KEY_DOMAIN_USER
0x00000U
|
|
|
The current version number of the stack tokens. MSB is the version, LSB is a complement.
|
|
|
|
#define
|
NVM3KEY_DOMAIN_THREAD
0x20000U
|
|
|
The current version number of the stack tokens. MSB is the version, LSB is a complement.
|
|
|
|
#define
|
NVM3KEY_DOMAIN_COMMON
0x80000U
|
|
|
The current version number of the stack tokens. MSB is the version, LSB is a complement.
|
|
|
|
#define
|
NVM3KEY_STACK_NVDATA_VERSION
(
NVM3KEY_DOMAIN_THREAD
| 0xFF01)
|
|
|
The current version number of the stack tokens. MSB is the version, LSB is a complement.
|
|
|
|
#define
|
NVM3KEY_STACK_BOOT_COUNTER
(
NVM3KEY_DOMAIN_THREAD
| 0xE263)
|
|
|
The current version number of the stack tokens. MSB is the version, LSB is a complement.
|
|
|
|
#define
|
NVM3KEY_STACK_NONCE_COUNTER
(
NVM3KEY_DOMAIN_THREAD
| 0xE563)
|
|
|
The current version number of the stack tokens. MSB is the version, LSB is a complement.
|
|
|
|
#define
|
CURRENT_STACK_TOKEN_VERSION
0x03FC
|
|
|
The current version number of the stack tokens. MSB is the version, LSB is a complement.
|
The tokens listed here are divided into three sections (the three main types of tokens mentioned in token.h):
-
Manufacturing
-
Stack
-
Application
For a full explanation of the tokens, see
hal/micro/token.h
. See
token-stack.h
for source code.
A set of tokens is predefined in the APPLICATION DATA section at the end of
token-stack.h
because these tokens are required by the stack, but they are classified as application tokens since they are sized by the application via its CONFIGURATION_HEADER.
The user application can include its own tokens in a header file similar to this one. The macro ::APPLICATION_TOKEN_HEADER should be defined to equal the name of the header file in which application tokens are defined. See the APPLICATION DATA section at the end of
token-stack.h
for examples of token definitions.
Since
token-stack.h
contains both the typedefs and the token defs, there are two #defines used to select which one is needed when this file is included. #define DEFINETYPES is used to select the type definitions and #define DEFINETOKENS is used to select the token definitions. Refer to token.h and token.c to see how these are used.
EM35x Microprocessors
HAL function names have the following prefix conventions:
halCommon:
API that is used by the EmberZNet stack and can also be called from an application. This API must be implemented. Custom applications can change the implementation of the API but its functionality must remain the same.
hal:
API that is used by sample applications. Custom applications can remove this API or change its implementation as they see fit.
halStack:
API used only by the EmberZNet stack. This API must be implemented and should not be directly called from any application. Custom applications can change the implementation of the API, but its functionality must remain the same.
halInternal:
API that is internal to the HAL. The EmberZNet stack and applications must never call this API directly. Custom applications can change this API as they see fit. However, be careful not to impact the functionalty of any halStack or halCommon APIs.
See also
hal.h
.
|
#define CREATOR_STACK_ALTERNATE_KEY 0xE475
|
|
#define CREATOR_STACK_ANALYSIS_REBOOT 0xE162
|
|
#define CREATOR_STACK_APS_FRAME_COUNTER 0xE123
|
|
#define CREATOR_STACK_BINDING_TABLE 0xE274
|
|
#define CREATOR_STACK_BOOT_COUNTER 0xE263
|
|
#define CREATOR_STACK_CERTIFICATE_TABLE 0xE500
|
|
#define CREATOR_STACK_CHILD_TABLE 0xFF0D
|
|
#define CREATOR_STACK_CLASSIC_DATA 0xE364
|
|
#define CREATOR_STACK_HOST_REGISTRY 0xE502
|
|
#define CREATOR_STACK_KEY_TABLE 0xE456
|
|
#define CREATOR_STACK_KEYS 0xEB79
|
|
#define CREATOR_STACK_NETWORK_MANAGEMENT 0xE125
|
|
#define CREATOR_STACK_NODE_DATA 0xEE64
|
|
#define CREATOR_STACK_NONCE_COUNTER 0xE563
|
|
#define CREATOR_STACK_NVDATA_VERSION 0xFF01
|
|
#define CREATOR_STACK_PSL_DATA 0xE501
|
|
#define CREATOR_STACK_TRUST_CENTER 0xE124
|
|
#define CURRENT_STACK_TOKEN_VERSION 0x03FC
|
Please see
hal/micro/token.h
for a more complete explanation.
|
#define DEFINE_BASIC_TOKEN
|
(
|
|
name,
|
|
|
|
|
type,
|
|
|
|
|
...
|
|
|
)
|
|
TOKEN_DEF
(name, CREATOR_##name, 0, 0, type, 1, __VA_ARGS__)
|
|
#define DEFINE_COUNTER_TOKEN
|
(
|
|
name,
|
|
|
|
|
type,
|
|
|
|
|
...
|
|
|
)
|
|
TOKEN_DEF
(name, CREATOR_##name, 1, 0, type, 1, __VA_ARGS__)
|
|
#define DEFINE_FIXED_BASIC_TOKEN
|
(
|
|
name,
|
|
|
|
|
type,
|
|
|
|
|
address,
|
|
|
|
|
...
|
|
|
)
|
|
|
Value:
TOKEN_DEF
(name, CREATOR_##name, 0, 0, type, 1, __VA_ARGS__)
#define TOKEN_NEXT_ADDRESS(region, address)
By default, tokens are automatically located after the previous token.
Definition:
token-stack.h:69
TOKEN_DEF
#define TOKEN_DEF(name, creator, iscnt, isidx, type, arraysize,...)
Definition:
cortexm3/token.h:197
|
#define DEFINE_FIXED_COUNTER_TOKEN
|
(
|
|
name,
|
|
|
|
|
type,
|
|
|
|
|
address,
|
|
|
|
|
...
|
|
|
)
|
|
|
Value:
TOKEN_DEF
(name, CREATOR_##name, 1, 0, type, 1, __VA_ARGS__)
#define TOKEN_NEXT_ADDRESS(region, address)
By default, tokens are automatically located after the previous token.
Definition:
token-stack.h:69
TOKEN_DEF
#define TOKEN_DEF(name, creator, iscnt, isidx, type, arraysize,...)
Definition:
cortexm3/token.h:197
|
#define DEFINE_FIXED_INDEXED_TOKEN
|
(
|
|
name,
|
|
|
|
|
type,
|
|
|
|
|
arraysize,
|
|
|
|
|
address,
|
|
|
|
|
...
|
|
|
)
|
|
|
Value:
TOKEN_DEF
(name, CREATOR_##name, 0, 1, type, (arraysize), __VA_ARGS__)
#define TOKEN_NEXT_ADDRESS(region, address)
By default, tokens are automatically located after the previous token.
Definition:
token-stack.h:69
TOKEN_DEF
#define TOKEN_DEF(name, creator, iscnt, isidx, type, arraysize,...)
Definition:
cortexm3/token.h:197
|
#define DEFINE_INDEXED_TOKEN
|
(
|
|
name,
|
|
|
|
|
type,
|
|
|
|
|
arraysize,
|
|
|
|
|
...
|
|
|
)
|
|
TOKEN_DEF
(name, CREATOR_##name, 0, 1, type, (arraysize), __VA_ARGS__)
|
|
#define DEFINE_MFG_TOKEN
|
(
|
|
name,
|
|
|
|
|
type,
|
|
|
|
|
address,
|
|
|
|
|
...
|
|
|
)
|
|
|
Value:
TOKEN_MFG(name, CREATOR_##name, 0, 0, type, 1, __VA_ARGS__)
#define TOKEN_NEXT_ADDRESS(region, address)
By default, tokens are automatically located after the previous token.
Definition:
token-stack.h:69
|
#define NVM3KEY_DOMAIN_COMMON 0x80000U
|
Please see
hal/micro/token.h
for a more complete explanation.
|
#define NVM3KEY_DOMAIN_THREAD 0x20000U
|
Please see
hal/micro/token.h
for a more complete explanation.
|
#define NVM3KEY_DOMAIN_USER 0x00000U
|
Please see
hal/micro/token.h
for a more complete explanation.
Please see
hal/micro/token.h
for a more complete explanation.
Please see
hal/micro/token.h
for a more complete explanation.
Please see
hal/micro/token.h
for a more complete explanation.
|
#define TOKEN_NEXT_ADDRESS
|
(
|
|
region,
|
|
|
|
|
address
|
|
|
)
|
|
|
If a token needs to be placed at a specific location, one of the DEFINE_FIXED_* definitions should be used. This macro is inherently used in the DEFINE_FIXED_* definition to locate a token, and under special circumstances (such as manufacturing tokens) it may be explicitely used.
-
Parameters
-
region
|
A name for the next region being located.
|
address
|
The address of the beginning of the next region.
|