EmberCommandState Struct Reference

For use when declaring a separate command streams. The fields are not accessed directly by the application.

#include < command-interpreter2.h >

Data Fields

uint8_t state
uint8_t buffer [ EMBER_COMMAND_BUFFER_LENGTH ]
uint16_t tokenIndices [ MAX_TOKEN_COUNT +1]
uint8_t tokenCount
uint16_t index
uint8_t error
uint8_t hexHighNibble
uint8_t argOffset
uint8_t previousCharacter
uint8_t defaultBase
EmberCommandEntry * currentCommand

Field Documentation

uint8_t EmberCommandState::argOffset
uint8_t EmberCommandState::buffer[ EMBER_COMMAND_BUFFER_LENGTH ]
EmberCommandEntry * EmberCommandState::currentCommand
uint8_t EmberCommandState::defaultBase
uint8_t EmberCommandState::error
uint8_t EmberCommandState::hexHighNibble
uint16_t EmberCommandState::index
uint8_t EmberCommandState::previousCharacter
uint8_t EmberCommandState::state
uint8_t EmberCommandState::tokenCount
uint16_t EmberCommandState::tokenIndices[ MAX_TOKEN_COUNT +1]

The documentation for this struct was generated from the following file:
  • command-interpreter2.h