AshRxState Struct Reference

#include < ash-v3.h >

Data Fields

uint8_t payload [ MAX_ASH_PAYLOAD_SIZE ]
uint8_t payloadIndex
uint8_t escapedPayloadIndex
uint8_t payloadLength
uint8_t controlByte
uint8_t headerEscapeByte
uint16_t computedCrc
uint8_t highCrcByte
uint8_t inBetweenCrcByte
AshRxFrameState frameState
bool escapeNextByte

The documentation for this struct was generated from the following file:
  • ash-v3.h