MacCountersData Struct Reference

#include < network-diagnostics.h >

Data Fields

uint16_t packetsSent
uint16_t packetsReceived
uint16_t packetsDroppedOnTransmit
uint16_t packetsDroppedOnReceive
uint16_t securityErrors
uint16_t numberOfRetries

Field Documentation

uint16_t MacCountersData::numberOfRetries
uint16_t MacCountersData::packetsDroppedOnReceive
uint16_t MacCountersData::packetsDroppedOnTransmit
uint16_t MacCountersData::packetsReceived
uint16_t MacCountersData::packetsSent
uint16_t MacCountersData::securityErrors

The documentation for this struct was generated from the following file:
  • network-diagnostics.h