EmberUdpConnectionData Struct Reference

Data stored for each connection.

#include < udp-peer.h >

Data Fields

EmberUdpConnectionHandle connection
uint16_t flags
uint16_t internal
uint8_t localAddress [16]
uint8_t remoteAddress [16]
uint16_t localPort
uint16_t remotePort

Field Documentation

EmberUdpConnectionHandle EmberUdpConnectionData::connection
uint16_t EmberUdpConnectionData::flags
uint16_t EmberUdpConnectionData::internal
uint8_t EmberUdpConnectionData::localAddress[16]
uint16_t EmberUdpConnectionData::localPort
uint8_t EmberUdpConnectionData::remoteAddress[16]
uint16_t EmberUdpConnectionData::remotePort

The documentation for this struct was generated from the following file:
  • udp-peer.h