Functions

bool emberZclClusterTimeClientTimeSyncCallback ( EmberZclDestination_t *timeServer)
Calls back user when a Network time server available.

Detailed Description

These callbacks are contributed by the Time Client plugin.

Function Documentation

bool emberZclClusterTimeClientTimeSyncCallback ( EmberZclDestination_t * timeServer )

This function is called from the client when a Time Server is available on the network.

Parameters
timeServer Pointer to the destination of the Time Server Ver.: always
Returns
FALSE if the application is not handling the update of Time Servers on this node.

References FALSE .