USB String Descriptor.

#include < em_usb.h >

Data Fields

uint8_t len
uint8_t type
char16_t name []

Field Documentation

uint8_t USB_StringDescriptor_TypeDef::len

Size of this descriptor in bytes.

char16_t USB_StringDescriptor_TypeDef::name[]

The string encoded with UTF-16LE UNICODE charset.

uint8_t USB_StringDescriptor_TypeDef::type

Constant STRING Descriptor Type.


The documentation for this struct was generated from the following file:
  • em_usb.h