Structure representing the AE (Application Event) data for BLE.
Public Attributes#
uint8_t AE_ADV_DATA_TYPE 1, AE_PERIODIC_ADV_DATA_TYPE 2, AE_SCAN_RSP_DATA_TYPE 3
uint8_t Advertising Handle, used to identify an Advertising set, Ranges from 0x00 to 0xEF
uint8_t Operation 0x00 - Intermediate fragment of fragmented extended advertising data.
uint8_t Fragment_Preference, Specifies the controller on where to fragment the Host advertising Data 0x00 - The Controller may fragment all Host advertising data.
uint8_t Data Length, Specifies Advertising_Data_Length , This parameter ranges from 0 to 251
uint8_t Data ,Specifies Advertising_Data.
Public Attribute Documentation#
type#
uint8_t rsi_ble_ae_data_s::type
uint8_t AE_ADV_DATA_TYPE 1, AE_PERIODIC_ADV_DATA_TYPE 2, AE_SCAN_RSP_DATA_TYPE 3
adv_handle#
uint8_t rsi_ble_ae_data_s::adv_handle
uint8_t Advertising Handle, used to identify an Advertising set, Ranges from 0x00 to 0xEF
operation#
uint8_t rsi_ble_ae_data_s::operation
uint8_t Operation 0x00 - Intermediate fragment of fragmented extended advertising data.
0x01 - First fragment of fragmented extended advertising data. 0x02 - Last fragment of fragmented extended advertising data. 0x03 - Complete extended advertising data. 0x04 - Unchanged data (just update the Advertising DID).
frag_pref#
uint8_t rsi_ble_ae_data_s::frag_pref
uint8_t Fragment_Preference, Specifies the controller on where to fragment the Host advertising Data 0x00 - The Controller may fragment all Host advertising data.
0x01 - The Controller should not fragment or should minimize fragmentation of Host advertising data.
data_len#
uint8_t rsi_ble_ae_data_s::data_len
uint8_t Data Length, Specifies Advertising_Data_Length , This parameter ranges from 0 to 251