You are viewing documentation for version:
Structure representing the BLE connection request.
This structure is used to define the parameters for a BLE connection request, which includes the address type and address of the device to connect, scan interval, scan window, connection interval, connection latency, and supervision timeout.
Public Attributes#
uint8_t
Address type of the device to connect.
uint8_t
Address of the device to connect.
uint16_t
Minimum connection interval.
uint16_t
Maximum connection interval.
Public Attribute Documentation#
dev_addr_type#
uint8_t rsi_ble_req_conn_s::dev_addr_type
Address type of the device to connect.
dev_addr#
uint8_t rsi_ble_req_conn_s::dev_addr[RSI_DEV_ADDR_LEN]
Address of the device to connect.
le_scan_interval#
uint16_t rsi_ble_req_conn_s::le_scan_interval
Scan interval.
le_scan_window#
uint16_t rsi_ble_req_conn_s::le_scan_window
Scan window.
conn_interval_min#
uint16_t rsi_ble_req_conn_s::conn_interval_min
Minimum connection interval.
conn_interval_max#
uint16_t rsi_ble_req_conn_s::conn_interval_max
Maximum connection interval.
conn_latency#
uint16_t rsi_ble_req_conn_s::conn_latency
Connection latency.
supervision_tout#
uint16_t rsi_ble_req_conn_s::supervision_tout
Supervision timeout.