Structure representing a BLE advertising request.
Public Attributes#
uint8_t
Advertising Status -.
uint8_t
Advertising type used during advertising -.
uint8_t
Advertising filter type -.
uint8_t
Address type of the device to which directed advertising has to be done -.
uint8_t
Address of the device to which directed advertising has to be done.
uint16_t
Advertising interval min 0x0020 to 0x4000.
uint16_t
Advertising interval max 0x0020 to 0x4000.
uint8_t
Address of the local device.
uint8_t
Advertising channel map.
Public Attribute Documentation#
adv_type#
uint8_t rsi_ble_req_adv_s::adv_type
Advertising type used during advertising -.
1. Advertising would visible (discoverable) to all the devices. Scanning/Connection is also accepted from all devices.
#define UNDIR_CONN 0x802. Advertising would be visible (discoverable) to the particular device mentioned in RSI_BLE_ADV_DIR_ADDR only.Scanning and Connection would be accepted from that device only.#define DIR_CONN 0x813. Advertising would be visible (discoverable) to all the devices. Scanning would be accepted from all the devices.Connection would be not be accepted from any device.#define UNDIR_SCAN 0x824. Advertising would be visible(discoverable) to all the devices. Scanning and Connection would not be accepted from any device.#define UNDIR_NON_CONN 0x835. Advertising would be visible(discoverable) to the particular device mentioned in RSI_BLE_ADV_DIR_ADDR only.Scanning and Connection would be accepted from that device only.#define DIR_CONN_LOW_DUTY_CYCLE 0x84
filter_type#
uint8_t rsi_ble_req_adv_s::filter_type
Advertising filter type -.
#define ALLOW_SCAN_REQ_ANY_CONN_REQ_ANY 0x00
#define ALLOW_SCAN_REQ_ACCEPT_LIST_CONN_REQ_ANY 0x01#define ALLOW_SCAN_REQ_ANY_CONN_REQ_ACCEPT_LIST 0x02#define ALLOW_SCAN_REQ_ACCEPT_LIST_CONN_REQ_ACCEPT_LIST 0x03
direct_addr_type#
uint8_t rsi_ble_req_adv_s::direct_addr_type
Address type of the device to which directed advertising has to be done -.
#define LE_PUBLIC_ADDRESS 0x00
#define LE_RANDOM_ADDRESS 0x01#define LE_RESOLVABLE_PUBLIC_ADDRESS 0x02#define LE_RESOLVABLE_RANDOM_ADDRESS 0x03
direct_addr#
uint8_t rsi_ble_req_adv_s::direct_addr[RSI_DEV_ADDR_LEN]
Address of the device to which directed advertising has to be done.
own_addr_type#
uint8_t rsi_ble_req_adv_s::own_addr_type
Address of the local device.
#define LE_PUBLIC_ADDRESS 0x00#define LE_RANDOM_ADDRESS 0x01#define LE_RESOLVABLE_PUBLIC_ADDRESS 0x02#define LE_RESOLVABLE_RANDOM_ADDRESS 0x03
adv_channel_map#
uint8_t rsi_ble_req_adv_s::adv_channel_map
Advertising channel map.
#define RSI_BLE_ADV_CHANNEL_MAP 0x01 or 0x03 or 0x07