Structure represents the BLE request for attribute descriptors.

This structure is used to define the parameters for a BLE request to get attribute descriptors, which includes the remote device address, the handle from which the search would start, and the handle at which the search would end.

Public Attributes#

uint8_t

Remote device address.

uint8_t

Search will start from this handle.

uint8_t

Search will end at this handle.

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_req_att_descs_s::dev_addr[RSI_DEV_ADDR_LEN]

Remote device address.


start_handle#

uint8_t rsi_ble_req_att_descs_s::start_handle[2]

Search will start from this handle.


end_handle#

uint8_t rsi_ble_req_att_descs_s::end_handle[2]

Search will end at this handle.