Structure represents the BLE command to set an attribute value.
This structure is used to define the parameters for a BLE command to set an attribute value, which includes the remote device address, the attribute handle, the length of the attribute value, and the attribute value itself. The module won't receive the acknowledgement from the remote device.
Public Attributes#
uint8_t
Remote device address.
uint8_t
Attribute handle.
uint8_t
Length of the attribute value.
uint8_t
Attribute value.