Structure represents the BLE GATT prepare write response.

This structure is used to define the parameters for a BLE GATT prepare write response, which includes the remote device address, the attribute handle, the attribute value offset, the length of the attribute value, and the attribute value itself.

Public Attributes#

uint8_t

Remote device address.

uint16_t

Attribute handle.

uint16_t

Attribute value offset.

uint16_t

Attribute value length.

uint8_t

Attribute value (data)

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_gatt_prepare_write_response_s::dev_addr[RSI_DEV_ADDR_LEN]

Remote device address.


handle#

uint16_t rsi_ble_gatt_prepare_write_response_s::handle

Attribute handle.


offset#

uint16_t rsi_ble_gatt_prepare_write_response_s::offset

Attribute value offset.


data_len#

uint16_t rsi_ble_gatt_prepare_write_response_s::data_len

Attribute value length.


data#

uint8_t rsi_ble_gatt_prepare_write_response_s::data[RSI_DEV_ATT_LEN]

Attribute value (data)