Structure represents the BLE Credit Based Flow Control (CBFC) connection response.

This structure is used to define the parameters for a BLE CBFC connection response, which includes the address of the remote device, the Local Channel Identifier (LCID), and the result of the connection request.

Public Attributes#

uint8_t

Address of the remote device.

uint16_t

Local Channel Identifier (LCID)

uint8_t

Result of the connection request.

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_cbfc_conn_resp_s::dev_addr[RSI_DEV_ADDR_LEN]

Address of the remote device.


lcid#

uint16_t rsi_ble_cbfc_conn_resp_s::lcid

Local Channel Identifier (LCID)


result#

uint8_t rsi_ble_cbfc_conn_resp_s::result

Result of the connection request.