Structure represents the BLE Credit Based Flow Control (CBFC) connection request.

This structure is used to define the parameters for a BLE CBFC connection request, which includes the address of the remote device and the Protocol/Service Multiplexer (PSM) value.

Public Attributes#

uint8_t

Address of the remote device.

uint8_t

Protocol/Service Multiplexer (PSM) value.

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_cbfc_conn_req_s::dev_addr[RSI_DEV_ADDR_LEN]

Address of the remote device.


psm#

uint8_t rsi_ble_cbfc_conn_req_s::psm

Protocol/Service Multiplexer (PSM) value.