Structure represents the BLE request for included services.

This structure is used to define the parameters for a BLE request to get included services, includes the remote device address, the handle from which the search would start, and the handle at which the search would end.

Public Attributes#

uint8_t

Remote device address.

uint8_t

Search will start from this handle.

uint8_t

Search will end at this handle.

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_req_inc_services_s::dev_addr[RSI_DEV_ADDR_LEN]

Remote device address.


start_handle#

uint8_t rsi_ble_req_inc_services_s::start_handle[2]

Search will start from this handle.


end_handle#

uint8_t rsi_ble_req_inc_services_s::end_handle[2]

Search will end at this handle.